STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC

I want to read  voltage of an  analog waveform  of 1khz after 50us of every rising edge and skip other reading of every cycle how to configure adc in stm32 if anyone have code for this please help.. 

ishu by Associate II
  • 1487 Views
  • 1 replies
  • 0 kudos

Simulink Support Package for Stm32 Discovery Board

Hello Community, I am using the hardware support package for STM32 in Simulink. I configured the timer and tried to use the timer block in Simulink but I am getting an error. can anyone help me find the root cause? I have attached the snap of the err...

Vcpkg issue

I'm using a VS Code extension that most probably uses `vcpkg`. After installing this extension, each time I run VS Code I get the following error:> Using vcpkg executable at "c:\Users\Luka\.vscode\extensions\ms-vscode.vscode-embedded-tools-0.7.0-win3...

lgacnik97 by Associate III
  • 4736 Views
  • 3 replies
  • 0 kudos

STM32WLE RTC AlarmA for wake-up from Standby

Hi , I need  for my applicetion two maner of wake-up from Standby mode. One is regular wake up every one hour and second is asynchronous wake up by external signal. I have used WKUP1 signal on  PA0 input for external wake up. It is working corectly o...

OM by Associate II
  • 1737 Views
  • 1 replies
  • 0 kudos

Resolved! Starting EXTI disabled

I've used CubeMX to enable in PA4 as in input with EXTI interrupt enabled on a STM32F373.  It works well, but how to I enable the device with this interrupt disabled by default?  HAL seems to enable the interrupt and then allow the 'user' code' to be...

LMorr.3 by Senior II
  • 3021 Views
  • 4 replies
  • 1 kudos

Resolved! STM32C011J4M6 trying to use HSE as clock

ok so when i debug and step through my code the hse ready bit in the rcc-cr register sets to one but when i run it it hangs at my while loop waiting for it to set why does this happen 

BLUENRG-M0A: Maximum Memory for Services/Characteristics

Hello,I am working with the Nucleo-f401re with the X-Nucleo-IDB05A2 expansion board for Bluetooth via BlueNRG-M0A module. I am trying to create services and characteristics for those services and I am trying to understand how the memory allocation po...

KMew by Senior III
  • 1834 Views
  • 1 replies
  • 0 kudos