STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! FIR-filter for STM32F4 and several frequency bands?

Hi,there are a lot of examples and tutorials available that describe how to use a FIR-filter (via function arm_fir_f32()). Unfortunately all these examples are either simple low-, high-, or bandpass-filters. Now what I'm looking for, is a possibility...

BSchm.6 by Associate III
  • 4784 Views
  • 4 replies
  • 1 kudos

Designing with STM32L496QGI6

Hello Team,We are planning to use the MCU STM32L496QGI6 for one of our new projects.The MCU will be powered from a 1.8V source (since all external peripherals are working in 1.8V only).One of the SPI slaves is working in 3.3V, so we are planning to u...

SVarg.2 by Associate
  • 985 Views
  • 1 replies
  • 0 kudos

Resolved! How can STM32F769 DMA controllers access the DTCM?

I am working with the STM32F769 microcontroller and I can see that a lot of DMA buffers are placed in DTCM in the source code I'm working with. Looking at the data sheet ( https://www.st.com/resource/en/datasheet/stm32f765bi.pdf ) page 20 I don't see...

arnold_w by Senior II
  • 2906 Views
  • 2 replies
  • 0 kudos

Stm32h7 HRtim input capture ability

Can I measure low pulse duration(>10ns) using the STM32H Hrtim?Hi all,I'm new to STM32H7 development. So I'm hoping to get some help to start.I need to measure pulse duration in 5- nanoseconds resolution or less. I then need to transfer the measured ...

Burakgvl by Associate II
  • 6297 Views
  • 4 replies
  • 0 kudos

STM32F2 USB HOST interrupt flood

Hello,I get an issue with the USB HOST configured on my STM32F2This USB HOST driver works well in my case, but it appears that the interrupt OTG_HS_IRQHandler is called too frequently (when I plug a device on the USB HOST post) and it's flooding my C...

jean by Senior
  • 1689 Views
  • 0 replies
  • 0 kudos

Resolved! HSE Oscillator for STM32L01 series MCU

I'd like to try using the STM32L011E4Y6TR in a new design.  However, the HSE input has only one pin (RCC_CK_IN) and I'm not sure how to use it with a standard 4 pin crystal that typically connects to 2 mcu pins.  Can someone point me toward a referen...

STM32H745 Timer 2 Triggering Prematurely when using ITR1

I have set up TIM2 as a slave triggered by ITR1,  But have not started any other timers to generate a suitable TRGO to trigger TIM2.  However, when I run the software I can see an output from TIM2 as soon as it is started.If I change TIM2 to be trigg...

NBrick67 by Associate II
  • 3743 Views
  • 6 replies
  • 0 kudos

Resolved! RTC 30 Feb

Hello st community, I work on stm32F4, and I use with RTC for date time.When I write in RTC a wrong day (for example 30 Feb 2023 or 31 Apr 2023) I havent a error in the result.It is possible to ask if the data is correct ?if (HAL_RTC_SetDate(&hrtc, &...

IlConte by Associate III
  • 2421 Views
  • 4 replies
  • 0 kudos

Printf Redirect on Multiple Core MCUs

Before starting out on further investigation, I'd like to ask if anyone has used a USART and printf redirect on BOTH cores at the same time? I'm under the impression that the "Resource Manager" library might be part of the solution, but really unclea...