STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H743BIT6 internal ADC with offset of +150mV

Hello alli have a board with STM32H743BIT6 on it with 4 INTERNAL ADC pin connected to resistor ladders.i connected external 2.5V reference and defined in the IOC file to use external reference.i have constant offset of +150mV and all readings of the ...

ZSade.1 by Associate II
  • 1363 Views
  • 1 replies
  • 0 kudos

STM32H743 SAI DMA noise

Hello,I took over working code that I have for a DSP project from an STM32F439 to an STM32H743. On the F4 I had the external audio codec connected to the I2S peripheral but switched over to the SAI on the H7. Now I am experiencing excessive noise whe...

Screenshot 2023-09-05 165736.png Screenshot 2023-09-05 170054.png Screenshot 2023-09-05 191001.png Screenshot 2023-09-05 191015.png
JP_ama by Associate III
  • 6064 Views
  • 1 replies
  • 0 kudos

STM32 SPI with CC1125 (TI)

The CC1125 is a TI sub-GHz transceiver: https://www.ti.com/product/CC1125The User's Guide - https://www.ti.com/lit/pdf/swru295 - says that, after asserting CS, the SPI Master must wait for the CC1125 to pull MISO low before starting the transfer:I th...

AndrewNeil_0-1692961715299.png

Data Transmitt and Receive through Ethernet(Nucleo H745ZI_Q)

Hello , I have a  Nucleo H745ZI_Q board  here Ethernet configuration and ping test done . Ping Test successfully ping's .Next i want send data from PC to Board  or  receive data  How and where should i process(in code - function )the data and how sho...

ETHping.jpj.png
SA  V.1 by Senior
  • 1319 Views
  • 2 replies
  • 0 kudos

Resolved! what is H5 IDAU configuration ?

I could not find yet a specific information regarding IDAU configuration of H5. Is it same as U5 as described in AN5347 ?Edit: I think it is the one in the reference manual (RM0481), I realized colors (Figure 2) indicate the IDAU mapping.

mete by Senior II
  • 1663 Views
  • 1 replies
  • 1 kudos

STM32G474RE Startup Issue

Hi everyone,I have a hardware problem with STM32G474RE on startup. If I try to supply this MCU directly from the lab power supply, it runs correctly, but when I have dips or drops or fast switching on the supply, I notice that the MCU doesn't start. ...

DKlew.1 by Associate
  • 1735 Views
  • 2 replies
  • 0 kudos

Echo cancellation on STM32F769I-DISCO

Hi, I need to perform a noise reduction and echo cancellation on an audio signal coming from an analog microphone and going out on a loudspeaker in order to make VOIP between 2 boards. I have an STM32F769I-DISCO board containing an STM32F769, a WM899...

PascalB by Associate
  • 2000 Views
  • 1 replies
  • 0 kudos

OV5640 Issue in JPEG mode

Hi,I try to use your OV5640 board with your OV5640 driver in STM32H747 BSP in JPEG mode.The problem is that the FPS drop to 1 or 2 even at low resolution QVGA.Can you show me what registers needed to be modified to make it work correct since your dri...

MSale.1 by Senior
  • 1872 Views
  • 1 replies
  • 0 kudos