STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to config track clock on NUCLEO-H563ZI

I am using the MDK-ARM tool to develop our application.When I enable the "Trace Exceptions" function to trace all exceptions, it always show "No synchronization" in red below. And no exception can be seen from the table.I also uploaded the trace cloc...

No_sync.png Trace_clock.png

Why should in 'G4 PB8/BOOT0 be set to non-Analog?

In 'G4 Datasheets and RM, the following remark can be read:It is recommended to set PB8 to a different mode than the analog one to limit theconsumption that would occur if the pin is left unconnected.This must be important, as it's at both in DS and ...

Analog Watchdog to wake the sleep mode in stm32

Hi, We use stm32f103c8t6 microcontroller. I need a output for Analog watchdog,adc read continuously background. I access analog value to activate sleep mode and wake up mode. I access the POT to Low threshold(0<100) to activate sleep mode and access ...

mrsmile by Associate III
  • 1657 Views
  • 0 replies
  • 0 kudos

Resolved! How to Convert UART received data into Float

HI"I am using an STM32G071CBT6 controller, and I am receiving data using the receive interrupt. I have received some values in my buffer memory, and now I want to convert them to float. If you have any examples, please share them. My buffer memory is...

suriya by Associate II
  • 8072 Views
  • 10 replies
  • 1 kudos

STM32F401RE

AREA mycode, CODE  EXPORT __mainmyclock EQU 0x40023830myDmode EQU 0x40020000myDout EQU 0x40020014myPU_PD EQU 0x4002080CmyPC13I EQU 0x40020810  ENTRY__main PROC  NOP;------------------------------Port C Clock Enable  LDR R1,=myclock  LDR R5,[R1]  MOV ...

CCV by Associate II
  • 1971 Views
  • 3 replies
  • 0 kudos

STM32F4 sometimes not booting correctly

Hello,I have a PCB that I have installed an STM32f407 or STM32f427. The PCB has CAN peripherals, serial peripherals, a status LED, a reset button and other peripherals.I have seen that on startup sometimes the STM32F4 doesn't startup correctly. When ...

RAugu.1 by Associate
  • 4517 Views
  • 7 replies
  • 2 kudos

Resolved! Irregular adc conversions triggered / synchronized by timer

Hi there!I'm working with a nucleo144-STM32F767zi and facing a problem with irregular ADC conversions (HAL_ADC_Start_IT) which are triggered by a eg. 50 kHz timer update event (every 20 us TIM1 fires an update event)ADC Clock prescaler seems to be PC...

lserrnt_1-1693572140484.png lserrnt_2-1693573420554.png lserrnt_0-1693572061169.png
lserrnt by Associate II
  • 4918 Views
  • 6 replies
  • 1 kudos

Resolved! Decoding the STM32H563 datasheet (RM0481 rev 1)

The MCU is great, but the datasheet (in particular the SPI section) is very hard to read. Whatever the original language was, it wasn't English, and I guess Google translate has been involved. I've added an example below, and hope for ST to update th...

Dimlite by Associate III
  • 2594 Views
  • 2 replies
  • 3 kudos

Nucleo F7 with Mic / Speaker Expansion Boards?

Hello,Strangely for the AEC AUD example cube pack, it lists the X-NUCLEO-F746ZG as a compatible CPU base in the getting started guid here: https://www.st.com/en/embedded-software/fp-aud-aec1.html#overview Call me blind, but the board connectors don't...