STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Circular DMA on ADC runs once and stops

I'm using an STM32H563. Setup to get ADC captures into a buffer using DMA in circular mode.I have TIM1 triggering an ADC1 conversion of two channels. And a buffer with 16 readings using DMA. The GPDMA is set in Standard Request Mode and Circular enab...

iguffick2 by Associate III
  • 3475 Views
  • 2 replies
  • 0 kudos

Resolved! STM32h725 Slave PSSI bad length

Hello,I'm trying to use the PSSI bus in slave mode to transmit data from a small FPGA. After some time chasing a weird bug (I'm losing 8 32bit words at the end of packet) I decided to use a logic analyzer on the bus and it showed a weird behavior fro...

mkhairy_0-1692434379099.png mkhairy_1-1692434419928.png USB_dump_start.png BUS_dump_start.png
mkhairy by Associate II
  • 11305 Views
  • 9 replies
  • 1 kudos

How to check CAN signal of CAN loopback mode in stm32f446RE

I have used an example code from STM of CAN loopback mode I have used a CAN transreceiver but i'm not getting how to check the signal as well as the data in CAN bus analyser please help me in hardware connection as well as how to check it in CAN bus ...

Komal by Associate III
  • 1036 Views
  • 0 replies
  • 0 kudos

how to print hello world in mcu boot using stm32f429zi board.

we r doing one task how to print hello world in mcu boot using stm 32 board . I KNOW THERE IS CONFIGURATION BUT NOT WORK properly we tried. there is one configuration CONFIG_BOOTLOADER_MCUBOOT=y which connect mcu boot code and application code. when...

VPati.2 by Associate II
  • 4040 Views
  • 7 replies
  • 0 kudos

Resolved! STM32F401 Datasheet Error? Vih

So table 54 Vih for 5V tolerant pins is 0.7Vdd. For Vdd 3.3V this is 2.31V.I'm having input capture trigger on signals that only reach 1.8V with 100% consistency on 4 pins.Most stm32f4 the Vih for the same pins is 0.45Vdd + 0.3V, which would be 1.65V...

TonyFauci by Associate II
  • 4995 Views
  • 9 replies
  • 3 kudos

Resolved! Excluding DMA from Scatter File CCM memory section

Hi, I have created scatter file: ; ************************************************************* ; *** Scatter-Loading Description File for STM32F4 *** ; ************************************************************* LR_IROM1 0x08004000 0x00...

JBond.1 by Senior II
  • 1552 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F44: UART Noise/Frame error with externel CPU clock

HiI have a self designed board (STM32F44 MCU) with an UART communication. It works well as long as I configure it to use the internal clock. As soon as I switch to the external clock (oscillator), the UART communication gives a noise and frame error ...

Corono_0-1696607734866.png
Corono by Associate III
  • 3839 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H7 | MPUs in dual cores

Hello @ all,I'm dealing with a project with stm32H755 MCU, as you know it is made of two cores: cortex-M7 and cortex-M4. Keeping in mind I'm using a few peripherals, among which FDCAN, SPI and most importantly lwIP/ETH, I'm trying to put together all...

Zzaaack by Associate III
  • 3360 Views
  • 3 replies
  • 3 kudos

HAL_TIM_Base_Start_DMA - STM32CubeMX

Posted on September 14, 2016 at 12:27I've try to use HAL_TIM_Base_Start_DMA with TIM6.To configure the system I'm using STM32CubeMX. We I start the project I can't receive any interrupt...HELP.In Attachment the ioc file.My change after code generati...