cancel
Showing results for 
Search instead for 
Did you mean: 

Bluepill to STM32F446 with CAN Bus

tictictoe
Associate

Hi. I have developed a CAN based protocol to a Bluepill and now I need to test that on the Nucleo board as well. I have been trying this for a while now and for some reason CAN messages are generated from the Nucleo board. The code was working fine with Bluepill and I need some guidance to change the paltform to Nucleo. PS:I am pretty sure that the custom built libraries are platform independent. 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0