STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB DFU configuration / use

Hi,I used a F105RCT6 in a custom board, i want to use the DFU mod.When I generate the project with cubemx I select USB DEVICE and DFU mid, i change the clock configuration corectly. I generate the FW, and i flash him.The DFU is running, i open cubepr...

Resolved! tolerance for the decoupling

I'm working on hardware design and have some doubts regarding selecting the tolerance value for the decoupling capacitor for stm32l4 series I have read the application note and data sheet I could not find the value for tolerance.so how can I find the...

vasikarans_0-1698914895304.png

sending same data over DMA

I'm using stm32u535 and LIS3DHTR accelerometer. The accelerometer has a 32 FIFO buffer, and I set it up so that it sends a signal to interrupt pin when FIFO is full. To read data, I need to send 0xE900,0x0000,0x0000 (saved in uint16_t  ACC_READ_ALL_D...

btd5 by Associate II
  • 1320 Views
  • 0 replies
  • 0 kudos

Resolved! Hardfault while using TrustZone STM32H573i-DK

Hi everyone,I'm currently experimenting with a STM32H573i-DK and TrustZone and facing some issues.First I tried enabling TrustZone in the Project Creation Process. When i try to run this empty project using the steps:SpoilerSelect and build the xxxxx...

funkii by Associate III
  • 2063 Views
  • 1 replies
  • 1 kudos

Resolved! What is the cause of erratum "2.10.6 Wrong ADC result if conversion done late after calibration or previous conversion"?

I have a mature project utilizing the STM32L4R5xxx series. The main function uses uC's ADC over about 15 channels. As a rule, the ADC readings are taken at a slow rate -- some triggered every 100 ms, others triggered every 5 seconds, and other trigge...

DDrin.1 by Associate II
  • 5108 Views
  • 7 replies
  • 1 kudos

Flexible SPI clock frequency

Hi,We have a need for arbitrary SPI clock frequencies. I looked at ~10 families and most STM32 micro-controllers seem to be limited to prescalers that divide the PCLK by a power of two. I found the STM32H7 but it is wildly over-specified for our appl...

pietrow by Associate
  • 1738 Views
  • 0 replies
  • 0 kudos

Wakeup from sleep or shutdown via TSC

Hello dear community. I am working on a project with a STM32L462CEU6 powered by battery. In this project we are also using TSC. Now I want STM32 to go in sleep or shutdown mode and wakeup when a touch pad has been touched. So the goal is that TSC mea...

Resolved! HRTIM 100% duty cycle

Hello,is there a solution to generate duty cycles between 0...100% with the HRTIM? I tried up-counting mode and center-aligned mode, but I wasn't able to achieve it. RegardsDominik Schmid

DSchm.3 by Associate II
  • 2352 Views
  • 1 replies
  • 0 kudos

Questions about how some HAL protocoles works in RTC

Hello ! I've been practicing how RTC works in STM32 Nucleo and I've used a code from this website tutorials.   void HAL_RTC_AlarmAEventCallback(RTC_HandleTypeDef *hrtc) { z ++; RTC_AlarmTypeDef sAlarm; HAL_RTC_GetTime(hrtc, &RTC_TimeStruct, FORM...

Xenon02 by Senior
  • 2235 Views
  • 5 replies
  • 2 kudos