STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 with Cortex-M85

Could it be time for ST to reveal such an MCU at the summit in a few weeks? Or maybe a Cortex-M55 that actually have integrated flash or MRAM or similar? (STM32N6 is interesting, but I would like to see flash/MRAM/something else integrated...

TLin.5 by Associate III
  • 828 Views
  • 3 replies
  • 4 kudos

Resolved! Configuration issue with Combined PWM mode on STM32F303RE

Hello everyone, I’m new to STM32 and I’m currently stuck with using timers.I’m working with an STM32F303RE, and the goal of my project is to generate 6 signals at 100 kHz (high time between 100 and 500 ns), each phase-shifted by 60°. These signals wi...

AB4 by Associate
  • 1043 Views
  • 3 replies
  • 4 kudos

ADC - TIMER - Sample rate confusion?

Hi, I need a little explanation about what is wrong behind my reasoning..I am using STM32F411. reading, two inputs of ADC in scan mode over circular DMA triggered via TIM2 update event.TIM2 is triggering ADC at 100KHz, so I have 50Khz sample rate per...

Bogdan_ST by Associate II
  • 1414 Views
  • 12 replies
  • 3 kudos

Resolved! Flash memory size of STM32H743XGH6

The STM32H743XGH6 is specified to have 1 MB of Flash memory.However, it seems that the following 2 MB address ranges are writable:BANK1: 0x08000000 to 0x080FFFFFBANK2: 0x08100000 to 0x081FFFFFIf the device really has only 1 MB of Flash, I would expec...

Resolved! STM32F303K8 ADC-DMA issue, DMA not firing

I have strange DMA problem with a F303 application, in particular a STM32F303K8 (a STM32F303x6/8 variant).The concept is relatively straightforward.A configured ADC sequence is triggered by timer, the ADC in turn triggers DMA transfers of the convers...

Ozone_0-1763372585585.png Ozone_1-1763372610827.png Ozone_2-1763372651567.png Ozone_4-1763372706496.png
Ozone by Principal III
  • 712 Views
  • 3 replies
  • 1 kudos

STM32F446RET6 DAC output

Hi, For STM32F446RET6, I want to use the DAC function of it. But I have some question. 1. If I don't use the output buffer, what is the output range? From the datasheet I think it should be 0.5mV to 3.3V±1LSB?2. If I use the output buffer, what is th...

Junzhe by Associate II
  • 637 Views
  • 3 replies
  • 0 kudos

14bit DCMI to 32MB SDRAM at 48MHz, on STM32H743IIT6

Hello dear ST forum.I need again you precious help.I am working on a data acquisition device, and need to get 14bit data from a parallel ADC connected on DCMI pins,at 48MHz, and move it to a 32MB SDRAM (W9825G6KH-6I) till almost full. The MCU is STM3...

nedelcu by Associate II
  • 1126 Views
  • 8 replies
  • 0 kudos

Using QSPI PSRAM with a STM32-H753 is that possible?

Hello,I am in the process of designing a product which is based on the STM32-H753 and requires P/SRAM.However, I'm concerned the H753 might not support on PSRAM with QSPI, I need the PSRAM for write/read.I haven't found any application notes or examp...

dvir1092_0-1763279213620.png dvir1092_1-1763279246874.png
dvir1092 by Associate II
  • 867 Views
  • 5 replies
  • 0 kudos