STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F103 VS MKI194V1(LSM6DSR)

Hi,I'm currently using the STM32F103 SPI to read the MKI194V1, but I've noticed that the ID I'm reading is always 0x4A. Could you please help me check if there's an issue, or provide any sample code?I also take a photo of the MKI194V1. The marking on...

S__119840846.jpg

Incorrect address of TIM1 in STM32NUCLEOF302R8

Recently while using the TIM1 feature in NUCLEOF302R8(DOCUMENT NUMBER:DS9896), I've found that the address was wrong in the datasheet but the address of TIM1 in SFR is correct when I tried the address in SFR's It worked.   I'll list the findings that...

SFR TIM1.png TIM1 addr_pages-to-jpg-0001.png

ADC Readings Lower than Ideal

I am using an STM32L562VET6Q MCU.  I have been having issues getting a valid reading from the ADC.  The signal is essentially DC (i.e., no fast high frequency measurements) so I conservatively set the ADC sampling time to its maximum.  My reference v...

patrickwright_0-1699541628321.png

Resolved! choosing flash latency vs. VOS

Giving an example for my question. For STM32H563, for freq. 140MHz, it is possible to use three different configurations:- 4 WS, VOS2- 4 WS, VOS1- 3 WS, VOS0If I want to optimize for power, I should choose 4WS VOS2. If I want to optimize for performa...

mete by Senior II
  • 1728 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U585 Azure IoT migrate to BG95

I'm trying to migrate my Azure IoT application from a BG96 to a BG95-M3, both from Quectel. I have solved some problem due to the difference in use of the uart3 pins of the BG96 and BG95. Should I make more modifications to the software? Is there a d...

JVica.1 by Associate II
  • 2560 Views
  • 3 replies
  • 0 kudos

Resolved! Real time changing AHB,APB1 Prescaler, Sampling frequency

Good evening,I am trying to sample various signals at different frequencies with adc in dma. Changing the size of the acquisition buffer seems inefficient, so I opted to change the clock prescalers, but it's giving me problems (I guess on changing th...

davidec by Associate III
  • 2133 Views
  • 2 replies
  • 1 kudos

Resolved! problem using PLL as SYSCLK over 200MHz on H5

I am trying to increase FCLK, and I changed the voltage scaling to VOS0, and configured the PLL1 for 240 MHz (src=HSI (HSIDIV=2), M=2, N=30, P=2), but it did not boot (it freezes when a change the system clock mux to PLL1). I realized when I decrease...

mete by Senior II
  • 2734 Views
  • 4 replies
  • 1 kudos