cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G070RB as Slave and ESP32 S3 C1 devkit as Master, I2C Bootloader

RamyaD
Associate II

Hi,

i am using STM32G070RB as Slave and ESP32 S3 C1 devkit as Master, Need to implement I2C Bootloader for stm32 from esp32. Can anyone help me with this.

 

Thanks in advance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee
If you want to program via I2C, you can use the internal bootloader and the AN4221 as a basis for your own development.
 
Hope that helps?
 
Regards /Peter
In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.