User Activity

Hi. I need help with RTC on STM32F103. I would like to edit the time (hours and minutes) in my RTC using a button. When I add an hour the maximum vartosc I can reach in the RTC->CNTL register is 65535 (18h20min), when this value is exceeded, the regi...
Hi. I have a problem with the RTC on STM32F103C6T6A. I wanted to add the ability to set the time. I would like to have a 24h clock. When CNTL overflows, CNTH does not increase making the clock reset close to 18h. void RTC_IRQHandler(void){ while ((RT...