Skip to main content
Associate
April 22, 2025
Solved

800KHz Frequency generation using STM32G070RBT6

  • April 22, 2025
  • 2 replies
  • 500 views

I am trying to get 800KHz frequency with Timer 3 and timer clock is 64MHz and i am using below setting to initalize the timer, but its frequency is 666.66KHz. Pls provide a solution of this problem ASAP......

 

static void MX_TIM3_Init(void)

{



/* USER CODE BEGIN TIM3_Init 0 */



/* USER CODE END TIM3_Init 0 */



TIM_ClockConfigTypeDef sClockSourceConfig = {0};

TIM_MasterConfigTypeDef sMasterConfig = {0};

TIM_OC_InitTypeDef sConfigOC = {0};



/* USER CODE BEGIN TIM3_Init 1 */



/* USER CODE END TIM3_Init 1 */

htim3.Instance = TIM3;

htim3.Init.Prescaler = 0;

htim3.Init.CounterMode = TIM_COUNTERMODE_UP;

htim3.Init.Period = 79;

htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

htim3.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;

if (HAL_TIM_Base_Init(&htim3) != HAL_OK)

{

Error_Handler();

}

sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

if (HAL_TIM_ConfigClockSource(&htim3, &sClockSourceConfig) != HAL_OK)

{

Error_Handler();

}

if (HAL_TIM_PWM_Init(&htim3) != HAL_OK)

{

Error_Handler();

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim3, &sMasterConfig) != HAL_OK)

{

Error_Handler();

}

sConfigOC.OCMode = TIM_OCMODE_PWM1;

sConfigOC.Pulse = 0;

sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

sConfigOC.OCFastMode = TIM_OCFAST_ENABLE;

if (HAL_TIM_PWM_ConfigChannel(&htim3, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)

{

Error_Handler();

}

/* USER CODE BEGIN TIM3_Init 2 */



/* USER CODE END TIM3_Init 2 */

HAL_TIM_MspPostInit(&htim3);



}
This topic has been closed for replies.
Best answer by TDK

This is quantization error in your logic analyzer. Increase your sampling rate to max or take the average of many different periods.

The timer settings and the output frequency are correct--look at the long term trend.

2 replies

TDK
TDKBest answer
April 22, 2025

This is quantization error in your logic analyzer. Increase your sampling rate to max or take the average of many different periods.

The timer settings and the output frequency are correct--look at the long term trend.

"If you feel a post has answered your question, please click ""Accept as Solution""."
ST Employee
April 22, 2025

Hello,

there should be set sConfigOC.Pulse value to non zero value to generate PWM on output pin. Try to set

sConfigOC.Pulse = 39;

 (50 % duty cycle).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.