STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Reading temperature from adc value(Non linear)

Hi,I am using STM32G491RE. I have to read temperature values from ADC. We  used voltage divider circuit to map the voltage values with temperature values it is non linear change between volatge and temperature.I tried below wayconst uint16_t adc_valu...

Resolved! STM32H735G-DK OCTOSPI2 HyperRAM 1st Read PASS, next Read FAIL

Hello,   I created the STM32H735G-DK project with the board selector in STM32CubeIDE. The OSPI_HyperRAM_MemoryMapped project was created by the example selector. Its HyperRAM test codes were added to the STM32H735G-DK project as below. The reading se...

JKim.2 by Senior
  • 3116 Views
  • 7 replies
  • 1 kudos

Resolved! FDCAN is not sending messages in Normal Mode

Good morning everyone,I’m trying to get FDCAN working on a STM32G431 however with very limited success. I’m not able to get a valid output signal on the TX line (measured with an oscilloscope) however, if I put the FDCAN peripheral into External Loop...

can send.png

Resolved! STM32U575: OCTOSPIM_P1_DQS in SDR mode?

I will use the STM32U575 with OCTOSPIM as Quad SPI (master) adapter.Q: The DQS signal is intended for DDR mode (I know).Could I use also DQS as input in SDR mode (when OCTOSPIM acts as SPI or QSPI master)?Idea:I want to compensate the "Round Trip Del...

tjaekel by Lead
  • 3284 Views
  • 6 replies
  • 1 kudos

stm32u545 OCTPSPI can't output wave in io pins

hello, I ues OCTOSPI device in STM32U545, it just generate cs and clock wave when run this code.HAL_OSPI_Command(hospi, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE)But io 0-3 nothing happened.I have reference the examples, it's use OCTOSPIM what not in...

LoganLi by Associate II
  • 2532 Views
  • 6 replies
  • 0 kudos

Problem with USB OTG FS (Device)

Hey everyone!Some context:We are developing a medical device using STM32H7ZIT6 MCU. We succesfully developed a working prototype, using UART connection protocol.  Couple of consistency problems (i.e. the device works flawlessly at times, sometimes we...

WhatsApp Image 2023-12-25 at 19.02.44.jpeg WhatsApp Image 2023-12-25 at 20.13.34.jpeg WhatsApp Image 2023-12-25 at 20.20.32.jpeg WhatsApp Image 2023-12-25 at 20.11.35.jpeg
CAdat.1 by Associate II
  • 3852 Views
  • 2 replies
  • 0 kudos