stm32h723vgh6 ethernet problem
Hi,
I have some problems with LwIp on custom board. Cpu type - stm32h723vgh6, ethernet chip - adin1200ccpz.
Phisical layer works fine (link led is up). I've generated cube project with UDP and ICMP support according to recommendations in example project STM32H723_Nucleo_ETH.
CORTEX M7 options
Speculation default mode ENABLE
CPU ICache ENABLE
CPU DCache ENABLE
Cortex memory protection region 1 settings
MPU region ENABLE
MPU region address 0x30000000
MPU region size 32KB
MPU SubRegion disable 0x0
MPU TEX field level level 1
MPU Access Permission ALL ACCESS PERMITTED
MPU Instruction Access DISABLE
MPU Shareability Permission DISABLE
MPU Cacheable Permission DISABLE
MPU Bufferable Permission DISABLE
Cortex memory protection region 2 settings
MPU region ENABLE
MPU region address 0x30000000
MPU region size 512B
MPU SubRegion disable 0x0
MPU TEX field level level 0
MPU Access Permission ALL ACCESS PERMITTED
MPU Instruction Access DISABLE
MPU Shareability Permission ENABLE
MPU Cacheable Permission DISABLE
MPU Bufferable Permission ENABLE
LwIP key options
MEM_SIZE (Heap Memory Size) 32232
LWIP_RAM_HEAP_POINTER (RAM Heap Pointer) 0x30000200
in liker file this part was added
/* ETH_CODE: add placement of DMA descriptors, rest is used by RX_POOL */
.lwip_sec (NOLOAD) :
{
. = ABSOLUTE(0x30000000);
*(.RxDecripSection)
. = ABSOLUTE(0x30000100);
*(.TxDecripSection)
} >RAM_D2
Sources in lan8742.c was modified to make it work with adin1200ccpz. MDIO requests from CPU woks fine. Data on rxd0 and rxd1 present.
Function low_level_input(struct netif *netif) constantly returns structure with tot_len and len fields 0 on any packet.
Ping - destination host unreachable (ICMP support - on).
Can anybody give me advice what to do?