STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1543 Views
  • 0 replies
  • 2 kudos

Resolved! cubeMX:access to example selector

When I open the official example using the example selector, CubeMX cannot display the graphical configuration of that example. I would like to know if it is possible to display the graphical configuration of the example in CubeMX. Thank you very muc...

stm64 by Associate II
  • 852 Views
  • 16 replies
  • 5 kudos

Resolved! CubeMX does not remember free pins generation context

STM32CubeMX v6.16.1 has a small bug. Under Project Manager - Code Generator - HAL settings is an option to pick under which context the free pins should be set as a analog. I am using STM32N6 which has 3 contexts (FSBL, App, ExtMemLoader).The problem...

MikkLeini_0-1768568318621.png

Resolved! stm32cubeMX is not starting

Hello,I was using STM32CubeMX, but starting two days ago, when I launch the program, only the splash screen appears and the STM32CubeMX does not proceed any further.1. I have tried deleting the program, restarting the computer, reinstalling it, and r...

modecs by Associate II
  • 743 Views
  • 9 replies
  • 1 kudos

Resolved! I2C rise and falltime setting

We have a board with a stm32u5. were VDDIO are connected to 1.8 V and  the I2C bus have pullup to 3.0 V. Some I2C devices uses 3.0 V logic levels and som 1.8 V. Between which voltage levels shall i measure the rise and falltime that i enter in cubemx...

Sebastian33_0-1764232564330.png Sebastian33_0-1764600090994.png