STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1592 Views
  • 0 replies
  • 2 kudos

Resolved! I2C rise and falltime setting

We have a board with a stm32u5. were VDDIO are connected to 1.8 V and  the I2C bus have pullup to 3.0 V. Some I2C devices uses 3.0 V logic levels and som 1.8 V. Between which voltage levels shall i measure the rise and falltime that i enter in cubemx...

Sebastian33_0-1764232564330.png Sebastian33_0-1764600090994.png

STM32CubeMX code generation mess with X-CUBE-FREERTOS

Hi there,I'm using an N6 with the latest version of IDE and MX with the FSBL/Appli dual project structure as per the FSBL LRUN template, and MX is incorrectly managing code. When using X-CUBE-FREERTOS in Application mode, code generation and cleanup ...

h7-v by Associate II
  • 531 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeMX CMake generator newlib-nano bug

Hello,I have observed this issue in version 6.16.1 across several MCU series (F3, F4, H5, H7), though it appears likely that all earlier versions are affected.The generated .cmake toolchain files incorrectly treat the --specs=nano.specs option as lin...