cancel
Showing results for 
Search instead for 
Did you mean: 

Alternate pin for I2C1_SCL on STM32C011J6Mx SO8N

stevecimo
Associate III

Hi ALL

I'm playing with a STM32C011J6Mx on  a plane breakout board.

Sorry if this a basic question, new to using the SMT32 , last time I played with MCUs was 6809 CPU :)

I wanted to use I2C and SWD, to use both I need to move the I2C1_SCL to it's alternate pin, when I CTL+ left click on the  PC15 (I2C1_SCL) it shows PA8 has an alternative.

stevecimo_0-1745539731667.png

But when I select PA8 , I2C_SCL , is not listed has an alternative function.

stevecimo_1-1745539814793.png

But the data sheet show it has a Alternate function on PA9, 

stevecimo_2-1745540364223.png

How do I activate PA9, in the MX tool?

 

Regards, Stephen

 

1 ACCEPTED SOLUTION

Accepted Solutions
stevecimo
Associate III

Never mind figured it out " the old use pin 9 instead of pin 11" trick :(

View solution in original post

1 REPLY 1
stevecimo
Associate III

Never mind figured it out " the old use pin 9 instead of pin 11" trick :(