User Activity

I am using the STM32L4 B-L475E-IOT01A board with the following modules:Wi-Fi module Inventek system ISM43362-M3G-L44Bluetooth module SPBTLE-RFDocumentation: https://www.st.com/resource/en/user_manual/um2153-discovery-kit-for-iot-node-multichannel-com...
Hi, I am using the STM32L4 B-L475E-IOT01A board with Wi-Fi module Inventek system ISM43362-M3G-L44.I have seen the example WiFi projects but they do not have the .ioc file. So my question is, is there any middleware available in STM32CubeMX which can...
Hi, I am using STM32MP257F-DK microcontroller. I have never used a dual cortex before. All I want to do is to generate a simple STM32CubeIDE project which also has a .ioc file. I want to debug it via CubeIDE.1) Do I need OpenAmp to successfully flash...
Hi,I am using STM32MP257-DK2 microcontroller on a Linux PC and I am trying to analyze a AI-model using the CubeAI. But I keep getting the following error:I have already installed the MP2 component, SDK and everything (including the CubeMX and CubeAI)...
Kudos from
Kudos given to