STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1570 Views
  • 0 replies
  • 2 kudos

STM32N6 RIF and MMT autoconfiguration errors

Reporting two issues when using STM32CubeMX v6.16.1 to generate STM32N6 code. I created new secure only template project for STM32N6570-DK to demonstrate the issue (it's attached).Only changes to the new project are these:In MMT defined RAM2 area ove...

MikkLeini_2-1769067127587.png MikkLeini_1-1769067113592.png

Migrating STM32F469NIH6 to STM32F769NIH6

I'm considering migrating from STM32F469NIH6 to STM32F769NIH6. From data sheets it is apparant that these two MCU's have compatible pinout, however the pinout compatibility tool of STM32CUBEMX V6.15.0 doesn't show these MCU's as compatible, why is th...

Resolved! Bug report: CubeMX on STM32WBA55CG with ThreadX

CubeMX version 6.16.1 I found STM32WBA55CG project with ThreadX,  the  parameter of "TX_LOW_POWER_USER_ENTER" and "TX_LOW_POWER_USER_EXIT" will be reset to default after the ioc re-open.This bug can be 100% reproduce. 

Kenwang by Associate III
  • 318 Views
  • 4 replies
  • 1 kudos

Generation of ports definition to main.h is inconvenient

Ports definition in main.h forced to include too mutch in dependend source files when one needs ports definition only.More convenient dedicated header file with ports definition only. Something like ports.h.It would be nice to have more layered struc...

vybor by Associate III
  • 334 Views
  • 4 replies
  • 3 kudos