2025-04-16 2:19 AM
Hello everyone,
I'd like to report some issues I encountered while using NetXDuo to create a UDP server with a Nucleo-N657X0-Q board:
After addressing all the issues above, I was finally able to get the UDP server working correctly!
Solved! Go to Solution.
2025-04-21 9:04 AM
Hello @LisaB
After check I confirm the issue and an internal ticket 208214 has been submitted to the dedicated team for fix.
For the 4th point, the tcp_sec and nx_data sections are not missing, but they need to be added manually as mentioned in this thread.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-16 2:29 AM
Hello @LisaB
Thank you for your contribution.
This issue is currently under investigation. I will get back to you as soon as possible.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-18 3:40 AM
Hello @LisaB
Can you include your IOC so that we can further investigate the issue?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-18 7:55 AM
Hello @Souhaib MAZHOUD,
sure, attacched the ioc file.
I configured in Stm32CubeIDE the UDP server as shown in the esample provided with the firmware STM32N6.
2025-04-21 9:04 AM
Hello @LisaB
After check I confirm the issue and an internal ticket 208214 has been submitted to the dedicated team for fix.
For the 4th point, the tcp_sec and nx_data sections are not missing, but they need to be added manually as mentioned in this thread.
BR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-09-28 1:31 AM
@Souhaib MAZHOUD Do you have any solution for the above issue?
I am trying to do the same with stm32n6570-dk board and facing the same issue: ethernet interface is grayed out in network interface settings in netxduo. Can you please check the status of the ticket and provide steps for the solution if have any.
Thanks,
Mani.
2025-10-26 5:27 AM
I have the same problem. Is there any solution?
2025-11-16 6:44 PM
I also have this issue.
2025-11-17 2:51 AM
The issue has been fixed, could you please check with the latest version of STM32CubeMX 6.16.0.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.