STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1547 Views
  • 0 replies
  • 2 kudos

ADC conversion mixing channels values

I'm working on a project in speed control of a pmsm and i am using ADC1 and 7 channels of the ADC to sample 7 different inputs. The ADC gets triggered from TIM2 and i'm doing the conversions every time i get a callback. At first the adc works fine wi...

Resolved! Make can not build project from STM32CubeMX with CMSIS_V2

I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everythi...

Michał M by Associate II
  • 1591 Views
  • 1 replies
  • 0 kudos

Resolved! Make can not build project from STM32CubeMX with CMSIS_V2

I encountered a problem with building project from STM32CubeMX v6.9.1 with generated Makefile and CMSIS_V2 enabled. Starting build by 'make' returns an error 1 for /main.o "Can not find specified file". On the other hand, when using CMSIS_V1 everythi...

Michał M by Associate II
  • 1842 Views
  • 2 replies
  • 0 kudos

STM32CubeMX 6.9.1 and STM32CubeIDE 1.13.1 released.

STM32CubeIDE 1.13.1 was released on st.com as well as an in-tool update patch aligned with STM32CubeMX v6.9.1 that is available for download.Main issues fixed in this patch:This patch release fixes the issues related to the following cases:STM32CubeM...

Resolved! LWIP - udp_new() returns PCB as NULL

Hi,I decided to upgrade my STM32CubeMX to the latest version 6.9.1.my project was generated first with STM32CubeMX 6.5.0 - so I had to copy the IOC manually.I checked multiple times that all configuration is the same like it was, and it is. when I'm ...

Mz.1 by Associate III
  • 4309 Views
  • 3 replies
  • 1 kudos

Disable auto comment generation

I understand the reason behind it and it is a very useful feature, but please add the option to disable it when it's not needed. Most of the time I just do a one-off configuration using the cube configurator and then I write my own code. Also, the wa...

BSerb by Associate II
  • 2152 Views
  • 2 replies
  • 0 kudos

Resolved! I don't know how to add the stm32cube expansion.

Hello.I am a student who is currently studying related to stm32 at the university.I'm learning how to install and use the program because it's my first time using the stm32 board.I would like to apply the expansion package that you gave me to the NUC...

Koseo.1 by Associate II
  • 3255 Views
  • 5 replies
  • 0 kudos