2022-12-21 3:07 AM
I installed CubeMX but i can't see the program when i try to search it on windows. Other ST programs can't see it too (Motor Control Workbench)
2022-12-21 3:46 AM
STM32CubeMX application is not available from the Program menu.
There was no desktop icon after install.
2022-12-22 2:02 AM
Hello @HYILD.1,
Please make sure to install the STM32CubeMX with admin rights. If you already did, you can navigate to the install folder "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX" and launch the STM32CubeMX.exe
Regards,
Chahinez.
2022-12-22 2:46 AM
Helle @ChahinezC
I can launch STM32CubeMX.exe from "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeMX"
But when I try to search it on program menu, there is no result for this.
I want to use ST Motor Control Workbench but when i try to generate code, it says no cubemx on computer.