STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1637 Views
  • 0 replies
  • 2 kudos

Disable auto comment generation

I understand the reason behind it and it is a very useful feature, but please add the option to disable it when it's not needed. Most of the time I just do a one-off configuration using the cube configurator and then I write my own code. Also, the wa...

BSerb by Associate II
  • 2212 Views
  • 2 replies
  • 0 kudos

Resolved! I don't know how to add the stm32cube expansion.

Hello.I am a student who is currently studying related to stm32 at the university.I'm learning how to install and use the program because it's my first time using the stm32 board.I would like to apply the expansion package that you gave me to the NUC...

Koseo.1 by Associate II
  • 3325 Views
  • 5 replies
  • 0 kudos

Resolved! system_stm32f4xx.c wrong code (SDRAM banks, GPIO_AFR)

HiI find these issues with the system_stm32f4xx.c file which CubeMX "generates":(a) CubeMX has Bank1, Bank2 enabled.  Code generated is only for Bank1.(b) CubeMX setting of pins (e.g/ AFR, MODER) does not match CubeMX Pinout.IOC attached.It seems tha...

MRobe.1 by Associate III
  • 2662 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeIDE & MX integrated

Hi,I have some problem with STM32CubeIDE, since when I start a new project everything works well as long as I delete the file: "home/STMCubeIDE/workspace_1-13.1/.metadata/.plugins/.org.eclipse.e4.workbench/workbench.xmi".However, when I exit the proj...

Fendo59 by Associate III
  • 14843 Views
  • 20 replies
  • 1 kudos

CDC_Standalone for STM32CubeU5

When will STM32CubeU5 have an example OTG_HS CDC_Standalone application?  I've use the example CDC_Standalone app from the many other STM32Cubes, but the M33 core appears to have a few significant differences.  Banging my head on the wall.That is, ST...

BillyBob by Associate II
  • 3214 Views
  • 3 replies
  • 0 kudos

Simulink and STM32H747XI

Anyone have a guide or how to setup a Arduino Giga R1 board in CubeMX with the intention to use with Matlab/Simulink? I found this online: https://github.com/szabo-tamas/GigaR1InitI have attempted to remove functionality for a more simplistic attempt...

Resolved! CubeMX problem when gen code for H563

making new project for H563 cpu has problems:1. output as makefile is greyed out - why ?2. output for stm32cubeIDE is possible, but output shows problem:what can i do now ?

AScha3_0-1693501411188.png
AScha.3 by Super User
  • 1656 Views
  • 2 replies
  • 0 kudos

Resolved! Pin assignments

Hi, I am using the Nucleo-F767ZI, when I am asigning a function to a pin (PD2) this make unselect the pin PG2, when I reassign the pin PG2 this makes the PD2 is deselected, the same when I try with the PF2, what is wrong? this using the graphic inter...