STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Resolved! STM32H725 SMPS issue

I am having and issue with a STM32H725RGV6.After powering my board, I can see the SMPS output at 1.36V, which I have connected to the VCAP inputs.I can also connect to the µC using the STM32CubeProgrammer.However, after flashing a simple firmware, th...

STM32H725RGV6 power.png
BenUtzer by Associate
  • 3378 Views
  • 3 replies
  • 2 kudos

Resolved! stm32cubeMX bug???

Hello,I am now using STM32CubeMX to config STM32G030F6P6, I want to use TIM14 to capture pulse, so I configged to Input Capture direct mode, which is obviously input port, but GPIO setting becomes GPIO output Low. is this a stm32cubeMX bug?please con...

dqsh06_0-1729747045042.png
dqsh06 by Senior
  • 2967 Views
  • 6 replies
  • 1 kudos

Resolved! Where in CubeMX can I check the Wait States?

Hi,I am using the STM32U5G9VJT6Q and in CubeMX I configured the clock to the full 160MHz for all busses including the core (first screenshot). According to the documentation for 160MHz I need to set 4 Wait States for those speeds and VCORE voltage ne...

Ricko_0-1741045992307.png Ricko_1-1741046086361.png
Ricko by Senior III
  • 1119 Views
  • 2 replies
  • 1 kudos

USBX DFU crashes dereferencing a NULL pointer

Good day all, USBX crashes at line 171 of the file ux_dcd_stm32_initialize_complete.c, as the dcd structure is not initialized at this point. I have tried this on two different MCUs, U575 and H753. In concert, on the H753 the code generator does not ...

DmitryR by Senior
  • 3100 Views
  • 9 replies
  • 4 kudos