cancel
Showing results for 
Search instead for 
Did you mean: 

Delay to Multi ADCs

giwonKIM
Associate III

 

HI.

 

I'm using 3ch in ADC3 of STM32H735VGT.

 

They are running in Continuous conversion mode without delay.

Do I have to give a delay after one conversion?

 

If so, how long should I delay?

 

Thank you.

 

 

static void MX_ADC1_Init(void)
{

/* USER CODE BEGIN ADC1_Init 0 */

/* USER CODE END ADC1_Init 0 */

ADC_MultiModeTypeDef multimode = {0};
ADC_ChannelConfTypeDef sConfig = {0};

/* USER CODE BEGIN ADC1_Init 1 */

/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;
hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 2;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.OversamplingMode = ENABLE;
hadc1.Init.Oversampling.Ratio = 10;
hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_NONE;
hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_CONTINUED_MODE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure the ADC multi-mode
*/
multimode.Mode = ADC_MODE_INDEPENDENT;
if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
sConfig.OffsetSignedSaturation = DISABLE;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_4;
sConfig.Rank = ADC_REGULAR_RANK_2;
sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */

/* USER CODE END ADC1_Init 2 */

}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
MM..1
Chief III

Place code as code and you show ADC1 no 3

sConfig.Channel = ADC_CHANNEL_5;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;

timing you can controll over sampling time or trigger any external or internal TIM.

Too sampling time 1.5 cycle is short and req low impedance source.

I'm converting once every 20us.

 

How much is appropriate?

 

 

Hello,

maximal sampling time you can use can be count for STM32H7, 12-bit resolution as:

 

ADC_SAMPLING_CYCLES <= (TIME_OF_CONVERSION * FREQUENCY_OF_ADC_KERNEL_CLOCK) - 6,5

 

where  TIME_OF_CONVERSION [s] is 20 us in your case, FREQUENCY_OF_ADC_KERNEL_CLOCK [Hz] is ADC clock and 6,5 is number of clock cycles needed for 12-bit resolution conversion. Than ADC_SAMPLING_CYCLES is the maximal number of sampling cycles you can use so choose in configuration the nearest lower number of sampling cycles.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.