User Activity

Posted on February 09, 2017 at 02:08I've got a custom board with a STM32F103 that connects to a micro SD card using 1 bit SDIO. I've generated some basic test code using STM32CubeMx Rev 4.19.0 and STM32CubeF1 release 1.4.0 (both the latest according...
Posted on October 20, 2014 at 02:18I've copied the SDRAM hardware and software from the STM32F429 Discovery board. We've made a few boards so far. On some the SDRAM doesn't seem to work at all while on others it seems to work for a bit then get corr...
Posted on November 01, 2012 at 06:41hi I'm using ST-LINK utility version 2.4.0 with STLinkUSBDriverdll V4.2.3.0 and ST-Link_CLI V1.4.0. I'm using Win 7 x64. I'm using a ST-Link V2 If I use it in ''automatic mode'' it seems to leak memory at an amazi...