STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1560 Views
  • 0 replies
  • 2 kudos

Resolved! STM32CubeIDE not generate code for GPIO pin

We are using the STM32WL55CCU6 processor and generating code for two cores. For GPIO it is not possible to specify which core will initialize the GPIO (of course, it is not necessary) but the code and definitions are not generated for any core.STM32C...

Entony_1-1741332753899.png
Entony by Associate II
  • 1775 Views
  • 1 replies
  • 0 kudos

STM32CubeMX shows conflicts for STM32F3348-DISCO

Hello,I am working on a project for the STM32F3348-DISCO board using STM32 IDE 1.18.0.I have created a new project with the following settings:- Target Reference: STM32F3348-DISCO- Firmware Package Name and Version: STM32Cube FW_F3 v1.11.5- Initializ...

Sati_0-1741290299579.png
Sati by Associate
  • 1187 Views
  • 2 replies
  • 0 kudos

UART get stuck in UART_WaitOnFlagUntilTimeout

Hi, I dont know the reason of this issue, I just generate code via STM32cubeMX after enabling UART4 and below there is the main program!: But my program cannot neither receive nor transmit any data and stuck in UART_WaitOnFlagUntilTimeout. Help pleas...

mmed by Associate III
  • 4767 Views
  • 12 replies
  • 1 kudos

CPU caches checkboxes blocked

 STM32H7 SeriesI have enabled generation of linker script (need to redefine memory layout).There is no possibility to change  state of checkboxes of both CPU caches if this generation has been enabled.The state of the checkboxes may be on or off, but...

trzeci by Associate III
  • 559 Views
  • 0 replies
  • 0 kudos

Resolved! CubeMX CAD models mixing LQFP144 and 208pinouts

Trying to export LQFP144 pinout to Altium CAD models with cubeMX.  But CubeMX is trying add pin #204 #202 #158, etc, on symbol for an L471 micro that doesn't even come in packages  bigger than 144 pins.  Altium chokes on this symbol, I imagine that's...

Screenshot 2024-10-21 180625.png
DixonDon by Associate II
  • 1352 Views
  • 2 replies
  • 0 kudos