STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

nRF24L01+ receiver problems

Hello,I am currently using a custom-built board designed to the nRF24L01+ specification and using the same exact circuit provided in their datasheet. It is connected to my STM32F103 through SPI. I am currently using this library to test out this boar...

Resolved! STM32L476 minimal ADC sampling time

Hello,STM32L476 data sheet Rev 8 talks in 3.15 about "Down to 18.75 ns sampling time" while table 77 only lists a minimal 31.25 ns minimal sampling time. Is 18.75 ns sampling time possible and with what setting?

Resolved! Read wrong content of MCU's internal flash

HelloI am working in dual bank mode with STM32G474RET6 MCU. I want to store some default values in internal flash beyond last programmed firmware's data address.For example I have following contents in flash (shown from STM32CubeProgrammer):Data star...

AlexHalf_0-1704730435486.png

Resolved! Getting problems with CAN on a NUCLEO-F207ZG Board

Hello everyone,   for a project I try to build a small CAN Bus with several Nucleo 144F207 Boards. Sadly, I have a really hard time to get it to work even though it should be rather simple. The minimum setup consists of two boards and two CAN Trancie...

CANconfig.PNG Scope1.jpg

Resolved! TSC Example

I am a begginer in the st enviroment, but still. I'm trying to use the touch sensing library, but there is very little good examples of how to just use one button as a sensor. I real all the documentation, still no good examples. I downloaded the lib...

mihaheh by Associate
  • 2975 Views
  • 3 replies
  • 0 kudos

NUCLEO-G071RB flash unlock hardfault

Hello,I'm new in ARM programming, I'm trying to study how CHIP work using the documentation.I wanna unlock the flash memory and according with documentation:1. Write KEY1 = 0x4567 0123 in the FLASH key register (FLASH_KEYR)2. Write KEY2 = 0xCDEF 89AB...

dmrsim by Associate III
  • 2014 Views
  • 4 replies
  • 1 kudos

Resolved! JTRST and NRST of STM32 MCU

Hello!What is the difference between JTRST and NRST of stm32 mcu?When using SWD, where should the RESET pin be connected? NRST or JTRST?

ellie99 by Associate
  • 6918 Views
  • 2 replies
  • 2 kudos

Resolved! STM32U575 : simple USB VCP UART

I have my own little board: with STM32U575CIT6Q (LQFP48 package). The USB is very simple and just DM (PA11) and DP (PA12) are connected. No USB-C, no USB-C Power Detector neither external chips for USB-C (as on NUCLEO-Board for USB-C-power).I want to...

tjaekel by Lead
  • 11627 Views
  • 17 replies
  • 1 kudos