STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G431: No FDCAN interrupts

I have two STM32 micros connected via CAN transceivers.  The sending unit is transmitting without issue, as evidenced by measuring both the CANH/CANL bus wires, as well as the CAN_RX/CAN_TX logical wires on the transmitter.  I did have to slow the bu...

Brian H by Senior
  • 2687 Views
  • 1 replies
  • 0 kudos

Resolved! while (!LL_SPI_IsActiveFlag_RXNE(EVE_SPI)) {} Never Returns

I'm trying to use SPI to communicate with a display (BT817) and whenever it tries to send data, the while (!LL_SPI_IsActiveFlag_RXNE(EVE_SPI)) {} never returns.  I've attached my CUBE IDE project.  Could anyone possibly give some guidance?  Am I miss...

No output on peripheral spi device

I'm trying to control a LTC-2668 dac device, through the spi interface. The dac opperates on mode 00 and spi commands are 24 bits long. The chip select pin is manually toggledThe thing is that even though the STM produces the correct output signals, ...

Στιγμιότυπο οθόνης (620).png 419990529_340221305639804_4347972341758977398_n.jpg 420513980_848781580380237_3177474528971993670_n.jpg

Resolved! STM32U575 PWR_S3WU IRQ

I am developing an application for the STM32U575, and am currently testing on the Nucleo-U575ZI-Q. As per the reference manual (Rev. 4) Section 10.9 PWR Interrupts, Table 110 Note 1: "The PWR_S3WU interrupt is generated only when the device is in Sto...

image.png
r-drage by Associate II
  • 3878 Views
  • 6 replies
  • 1 kudos

Uart bulk data transfer

Helloi need some help in transfering 24 bit 3 channel adc captured data via uart. SPI based ADC sampling rate is 4ksps i.e. I get dataready interrupt at every 256usec . The total bits per second would be then 4000x9x8 equals 288000.Can anyone help me...

prsh by Associate II
  • 2090 Views
  • 2 replies
  • 1 kudos

STM32H5 GPIO toggling performance

I use STM32H562 and/or STM32H503 (nucleo board). When try in loop only this line: while (1) {   GPIOB->ODR ^= GPIO_PIN_6;     } The frequency on pin is only 12.5 mhz. I use external quartz 8mhz (and 24mhz on nucleo) I config  to 250mhz (with build...

Brussl by Associate III
  • 9094 Views
  • 19 replies
  • 1 kudos

Resolved! ADC3 data DMA transfer error

Hello members,I have problem with functionality of DMA data stream for ADC3 peripheral. I have H743ZIT controller. ADC1 with DMA is fully and properly working for each channel. I have placed ADC data array to RAM_D2 section for ADC1. For ADC3 I have ...

sagit_0-1705511284067.png sagit_1-1705511325451.png
sagit by Associate II
  • 7317 Views
  • 8 replies
  • 0 kudos