STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G0B1KET6 CAN Bus-error

Now I've been sitting here for 2 long day's and still haven't been able to solve the BUS-error problem. I'm logging with Kvaser USB CAN card so what I want to see right now is some healthy frames coming out from it, but no, only bus-errors, so I thou...

JSVENS3_0-1762894629986.png JSVENS3_1-1762894931164.png
JSVENS3 by Associate II
  • 1004 Views
  • 6 replies
  • 0 kudos

Do FSK or PSK using HRTIM on STM32G474RE

Hello everyone, I'm trying to do FSK and PSK modulation using HRTIM in STM32G474RE but I have what I want when I use Oscillo to display. For example,  '1' = 45 kHz and '0' = 55 kHz. I want to transmit the message "1010" where each bit is 10µs long (F...

mala by Associate II
  • 2832 Views
  • 6 replies
  • 0 kudos

Resolved! STM32F303CCT6 vs STM32F303CBT6

I recently purchased some STMF303 boards for implementing a free pre-compiled HEX file.I received the boards with the STM32F303CCT6 chip, but the pre-compiled file was for the STM32F303CBT6 chip. The HEX loads but does not run on any 303CCT6.Are ther...

Resolved! How to use ADC with DMA on the STM32H7S78-DK

Hi everyone,I am currently trying to use the ADC with DMA on my STM32H7S78-DK. To do so, I am following this guide: https://community.st.com/t5/stm32-mcus/stm32h7r-s-how-to-configure-an-adc-dma-transfer-in-circular-mode/ta-p/737149. I've made little ...

VPguy by Associate II
  • 1086 Views
  • 4 replies
  • 0 kudos

Resolved! Running STM32U083 directly from Li-SOCL2 battery

I am using STM32U083 MCU in a project that runs on a 3.6v Li-SOCL2 lithium thionyl chloride battery (OC voltage 3.65V / Nominal voltage at 1mA 3.6V).Currently I have used a LDO of 2.5v to power the MCU, but I was thinking if we can eliminate the LDO ...

Magvel_0-1764049899520.png Magvel_1-1764049925505.png
Magvel by Associate II
  • 867 Views
  • 4 replies
  • 1 kudos

Resolved! Stm32N6 Core is locked

So i'm following along with this video* https://www.youtube.com/watch?v=usQ_f6Swpok&list=PLTJzs51NlEICI7ARAHOyUqMhTgJE0UFv0&index=5 I have the same* STM32N6-DK board This is my build command for the GPIO_IO_Toggle application.* /opt/st/stm32cubeide_1...

TheCoreIsLocked.png ProgrammingOutput.png

TIM 1 Advanved timer sometimes goes high

Hey!I will explain my setup and then paste the code. I have three different timers (TIM1, TIM2, TIM3) sending out PWMs to different parts of my board. All timers are set up the same way; the only difference is that TIM1 is an advanced timer.What I do...

morris by Associate III
  • 748 Views
  • 6 replies
  • 1 kudos