cancel
Showing results for 
Search instead for 
Did you mean: 

Sample code for the application note -AN5978

sudong
Associate
2 REPLIES 2
Chris21
Senior III

The document at the link you supplied says:

Before opening the STM32CubeMX ‘ioc’ file, make sure that the X-CUBE-DPOWER pack has been installed.
• Download the pack at https://www.st.com/en/embedded-software/x-cube-dpower.html
• Open the help tab and install the pack.

.

.

.

Once the pack has been installed, it is possible to check, change, modify the default workspace, and generate the
code for the IAR, Keil® or STM32CubeIDE compiler toolchains using the tab GENERATE CODE in the main
interface.

I have installed the DPower pack, but where can I find the sample project file?