STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Issues writing float data to UART

Hello everyone!Ran into some issues writing float data to the UART. I know with Nordic, there was some weird workaround that had to be used to convert it that looked something like this: NRF_LOG_INFO("MLX90393 X = " NRF_LOG_FLOAT_MARKER "\r", NRF_LO...

JayDev by Senior II
  • 5933 Views
  • 10 replies
  • 0 kudos

Isolation between digital 3.3V and Analog 3.3V supply

Hi @Peter BENSCH  Greetings again. I am using STM32H5 and STM32G4 series MCU in my project. As per the datasheets and application notes, it is recommended to isolate analog and digital supply voltages with a proper ferrite bead or a zero ohm resistor...

Wrong timer section identifier in manual (G431RBT6)

I think there are some wron identifiers?After reading the manual and seeing the tables i think it must be "tim_ti2_in0", "tim_ti3_in0" and "tim_ti4_in0" on page 1223? Also in the table on page 1081, there is a "tim_ti2_in[15:1]" that should be "tim_t...

Tobe by Senior III
  • 1124 Views
  • 1 replies
  • 0 kudos

Resolved! STM32G431 tim_ker_ck, tim_pclk source

I'm looking into calculating the timings for the brk filters for the TIM1 periphery. Mentioned there is the "tim_ker_ck" and the "tim_pclk" respectively.I cannot seem to find any information on where these come from.The clock tree in the RM says that...

DMeie.2 by Senior II
  • 4781 Views
  • 10 replies
  • 7 kudos

Resolved! NUCLO-H755ZI-Q Unable to debug CM4

Hi community,I build and program both CM without error and debugger configuration as in the AN5361 .The Nucleo- runs with maximum frequency  480 MHz, and Power supply:  HAL_PWREx_ConfigSupply(PWR_SMPS_2V5_SUPPLIES_LDO);  __HAL_PWR_VOLTAGESCALING_CONF...

Vero by Associate III
  • 3179 Views
  • 4 replies
  • 0 kudos

Resolved! Drop voltage SCL I2C

Hello,I have a very strange behaviour with the I2C bus of a STM32G431.I try to communicate with a MLX90393 of Melexis. I had some problems to get the measurements, after a Start measurement. The MLX90393 returned an error code. So I checked the signa...

0693W000007ZmIBQA0.png 0693W000007ZmIVQA0.png
alxrey by Associate II
  • 4691 Views
  • 6 replies
  • 0 kudos