cancel
Showing results for 
Search instead for 
Did you mean: 

two independent CAN

UVagl.1
Associate II

HI,
I'm working with a micro from the H7 family (H723).
I have to implement CAN communication on two distinct peripherals (FDCAN1 and FDCAN2) in interrupt mode but the system doesn't work.
Below are the settings I use in my project:

void MX_FDCAN2_Init(void)
{
  /*USER CODE BEGIN FDCAN2_Init 0 */
  /*USER CODE END FDCAN2_Init 0 */

  /*USER CODE BEGIN FDCAN2_Init 1 */
  /*USER CODE END FDCAN2_Init 1 */

  hfdcan2.Instance = FDCAN2;
  hfdcan2.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
  hfdcan2.Init.Mode = FDCAN_MODE_NORMAL;
  hfdcan2.Init.AutoRetransmission = DISABLE;
  hfdcan2.Init.TransmitPause = ENABLE;
  hfdcan2.Init.ProtocolException = DISABLE;
  hfdcan2.Init.NominalPrescaler = CAN_PRES;
  hfdcan2.Init.NominalSyncJumpWidth = CAN_SJW;
  hfdcan2.Init.NominalTimeSeg1 = CAN_T1;
  hfdcan2.Init.NominalTimeSeg2 = CAN_T2;
  hfdcan2.Init.DataPrescaler = CAN_DATA_PRES;
  hfdcan2.Init.DataSyncJumpWidth = CAN_DATA_SJW;
  hfdcan2.Init.DataTimeSeg1 = CAN_DATA_T1;
  hfdcan2.Init.DataTimeSeg2 = CAN_DATA_T2;
  hfdcan2.Init.MessageRAMOffset = 0;
  hfdcan2.Init.StdFiltersNbr = 1;
  hfdcan2.Init.ExtFiltersNbr = 0;
  hfdcan2.Init.RxFifo0ElmtsNbr = 5;
  hfdcan2.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan2.Init.RxFifo1ElmtsNbr = 2;
  hfdcan2.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
  hfdcan2.Init.RxBuffersNbr = 0;
  hfdcan2.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
  hfdcan2.Init.TxEventsNbr = 0;
  hfdcan2.Init.TxBuffersNbr = 0;
  hfdcan2.Init.TxFifoQueueElmtsNbr = 32;
  hfdcan2.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
  hfdcan2.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
  if (HAL_FDCAN_Init(&hfdcan2) != HAL_OK) {
    Error_Handler();
  }

  void MX_FDCAN1_Init(void)
  {
    /*USER CODE BEGIN FDCAN1_Init 0 */
    /*USER CODE END FDCAN1_Init 0 */

    /*USER CODE BEGIN FDCAN1_Init 1 */
    /*USER CODE END FDCAN1_Init 1 */

    hfdcan1.Instance = FDCAN1;
    hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
    hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
    hfdcan1.Init.AutoRetransmission = DISABLE;
    hfdcan1.Init.TransmitPause = ENABLE;
    hfdcan1.Init.ProtocolException = DISABLE;
    hfdcan1.Init.NominalPrescaler = CAN_PRES;
    hfdcan1.Init.NominalSyncJumpWidth = CAN_SJW;
    hfdcan1.Init.NominalTimeSeg1 = CAN_T1;
    hfdcan1.Init.NominalTimeSeg2 = CAN_T2;
    hfdcan1.Init.DataPrescaler = CAN_DATA_PRES;
    hfdcan1.Init.DataSyncJumpWidth = CAN_DATA_SJW;
    hfdcan1.Init.DataTimeSeg1 = CAN_DATA_T1;
    hfdcan1.Init.DataTimeSeg2 = CAN_DATA_T2;
    hfdcan1.Init.MessageRAMOffset = 0;
    hfdcan1.Init.StdFiltersNbr = 1;
    hfdcan1.Init.ExtFiltersNbr = 0;
    hfdcan1.Init.RxFifo0ElmtsNbr = 5;
    hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
    hfdcan1.Init.RxFifo1ElmtsNbr = 0;
    hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
    hfdcan1.Init.RxBuffersNbr = 0;
    hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
    hfdcan1.Init.TxEventsNbr = 0;
    hfdcan1.Init.TxBuffersNbr = 0;
    hfdcan1.Init.TxFifoQueueElmtsNbr = 32;
    hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
    hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_8;
    if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK) {
      Error_Handler();
    }

    void FDCAN_Config(FDCAN_HandleTypeDef * hfdcan)
    {
      FDCAN_FilterTypeDef sFilterConfig;

      /*Configure Rx filter */
      sFilterConfig.IdType = FDCAN_STANDARD_ID;
      sFilterConfig.FilterIndex = 0;
      sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
      sFilterConfig.FilterType = FDCAN_FILTER_RANGE;

      // sFilterConfig.FilterID1 = 0x83;
      // sFilterConfig.FilterID2 = 0x83;
      sFilterConfig.FilterID1 = 0x01;
      sFilterConfig.FilterID2 = 0x770;

      while (HAL_FDCAN_ConfigFilter(hfdcan, &sFilterConfig) != HAL_OK) { }

      /*Configure global filter:
      Filter all remote frames with STD and EXT ID
      Reject non matching frames with STD ID and EXT ID */

      while (HAL_FDCAN_ConfigGlobalFilter(hfdcan, FDCAN_REJECT, FDCAN_REJECT,
                 FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE)
          != HAL_OK) { }

      /*Start the FDCAN module */
      while (HAL_FDCAN_Start(hfdcan) != HAL_OK) { }
      while (HAL_FDCAN_ActivateNotification(
                 hfdcan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0)
          != HAL_OK) { }
    }
 
in main.c, i call FDCAN_Config(&hfdcan1) and FDCAN_Config(&hfdcan2) after MX_FDCAN1_Init() and MX_FDCAN2_Init().
 
Can anyone help me?
Thank you
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Use the </> tool to paste code, you can also edit posts. Perhaps add the whole project as a .ZIP or on GitHub?

>>..but the system doesn't work.

That's not a helpful description of the problem. You're going to need to refine that a little.

You'll need to review the circuit, how the peripherals configured/behaving at the register level in the debugger. The interrupt handlers and call backs are not shown.

Make each work independently first, perhaps in Loop Back mode.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

@UVagl.1 I've had the inserted code prettied up by a C Beautifier - it looks much more readable, doesn't it?

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.