STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm32f429igt6-ltdc-lvgl

DescriptionIam using stm32f429igt6 board for displaying an image using ltdc display. I have used lvgl library for displaying an image. For 16bit RGB565 format lvgl V7.4 worked well and good but i want V9.1 in which 24 RGB666 format is available. I ha...

[STM32H5] ADC clock configuration for different ADCs

Hi, I am using both ADC1 and ADC2 for my project. I want both the ADCs to be configured with different Prescalar . But by doing so I am observing ADC2 working with the ADC1 Prescalar. Why am I facing this issue? Is it possible to configure both the A...

Anusha by Associate
  • 2631 Views
  • 4 replies
  • 0 kudos

Resolved! Embedded bootloader and HAL

Dear all.I've implemented a M3 and M4 program ( drive a iLi display and 485 port) now I'm porting it to the H5 (H562RGTX).One of the latest issue I'm facing is the jump from bootloader to application. In M3/M4 i used only LL, and the jump has no prob...

TheRaprus by Associate III
  • 2867 Views
  • 3 replies
  • 1 kudos

Resolved! CAN and USB on STM32767ZiT6

Hello,I have a custom board based on STM32767ZIT6 and it has the three CAN peripherals and the USB designed. The goal is to translate the CAN message to USB directly without the need for a bridge but I am facing issues activating the USB and the thre...

WIF by Associate II
  • 9323 Views
  • 11 replies
  • 2 kudos

Typical pull-up resistance value

Hi, Greetings @Peter BENSCH  I am using STM32G431MB controller in my project. I am configuring PB4 as my General purpose Input pin. Ports PB5-PB9 as well as PC8,PC9, PA8 and PA9 are assigned as General purpose outputs connected to Analog HART Mux. In...

DFSDM in STM32F412CEUX

Dear STI am using an STM32f412CEUX(UFQFPN48) STM32f412CEUX's the PB1( DFSDM_DATAIN0) and PB2(DFSDM1_CKIN0) of STM32f412CEUX is connected digital Microphone I want to get audio signal through STM32f412CEUX's DFSDM Block But I can not find DFSDM1_CKOUT...

hongjo by Associate II
  • 2323 Views
  • 4 replies
  • 1 kudos

SSD1306 stop working while DMA Mode enabled to read ADC.

I am trying to read 4-20mA Transducer using ADC and DMA Enabled. Normally OLED works fine. But when i enabled DMA, OLED is blank. What could be wrong ?   int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration-----...

asking by Associate III
  • 1896 Views
  • 1 replies
  • 0 kudos

How to configure FIR filter in FFT USING NUCLEO-H745ZI

Hello Team,I'm trying to configure FIR filter in FFT in one point I am getting grab data every time in every call back collecting 1024 data and process to arm_fir_f32(); Function, is there any code related to this FIR filter in FFT.PFA code and sin w...

ggowd.1 by Associate III
  • 3599 Views
  • 3 replies
  • 0 kudos