STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Need a help About ITM_Sendchar

i can use ITM_SendChar with printf by overriding __io_putchar but currently i am working with C++ is there any way to use ITM_SendChar with cout? if there any can anyone please tell me how to do that or provide the code for that.Thanks in Advance

Asraful by Associate III
  • 2189 Views
  • 1 replies
  • 0 kudos

Stlink v3 minie problem

Hello everyone. I had some interesting issues with my stlink. I was debugging just fine for about 2–3 weeks, but yesterday i was unable to debug for several reasons: target under reset, cannot erase flash. But after a few hours, everything became fin...

zsx by Associate II
  • 2154 Views
  • 3 replies
  • 1 kudos

CAN communication

I want to establish can communication on CAN1 in which message being transmitted ,after every 5 m,/s. Below is my main.c and mcu.c . This is mcu.c file.     #include "Mcu.h" #include "Mcu_Config.h" #include "Mcu_Internal.h" #include "Mcu_RegTypes.h" ...

Resolved! STM32L0 standby mode current consumption optimization

Posted on August 02, 2017 at 10:52 Hello there. I am currently developing a coin cell powered device with the STM32L051C8. The datasheet says in standby mode the consumption is about 0.27uA (270nA). My current board only consists of a Voltage ...

Rob Keck by Associate II
  • 4305 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H723 Power Monitor Temperature and VBAT

All:The STM32H723 has a temperature sensor as part of PWR.Some questions:1. The HAL instruction to enable is HAL_PWREx_Enable_Monitoring( ) - can temperature be enabled independently of VBAT?2. Can TEMPL and TEMPH be changed, or are these permanently...

ToddA by Associate II
  • 3078 Views
  • 4 replies
  • 4 kudos

SD Card Init

Hello,I'm implementing the management of an SD Card using a micro STM32H7xx. While analyzing the SD Card initializaion procedure I came across the 'switch voltage' mechanism. I was wondering if anyone is aware of the timing associated with this aspec...

STM32 ADC dual regular simultaneous mode

I need to use dual regular simultaneous mode as I am using ADC1 and ADC2 simultaneously. I have enabled DMA for the both ADCs.When I am running below code in debug mode it is going into hard fault after halfconversioncplt function. It is not going in...

AKhot.1 by Senior
  • 9539 Views
  • 7 replies
  • 0 kudos

UCPD SINK Application NUCLEO-u575ZI-Q

I'm trying to run a simple UCPD SINK application on the NUCLEO-U575ZI-Q.I attempted to follow the example provided here: https://wiki.stmicroelectronics.cn/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink#-5BOPTIONAL-5D_Conf...

acipriano_1-1713372587747.png acipriano_2-1713372661433.png
acipriano by Associate II
  • 5218 Views
  • 10 replies
  • 0 kudos

stm32l-discovery weird blinking on LD1

Posted on March 12, 2014 at 02:49Hi all,Does anyone know what COM (LD1) LED on top of the STM32L-discovery board indicate??? I know that when we upload the code, it will blink in red and green very fast, and when it's powered on and work normally it...

readout protection without power on reset

Dear support team, I need to activate and deactivate the readout protection on a fully automated CI enviroment and according to the RM0440 (Note: If the read protection is set while the debugger is still connected through JTAG/SWD, applya POR (power-...