STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

firmware verification

Hello,I want to add a software update feature to my device, but I am unsure about the correct way to verify a newly installed firmware image. My goal is to make sure that the entire firmware has been written correctly and is not corrupted before the ...

scotzap by Associate II
  • 531 Views
  • 1 replies
  • 1 kudos

Resolved! Warning: The core is locked up

Hi,I am getting a warning "The core is locked up" and a few more (please refer to the attached image).I have also tried flashing with the hex file, but some flashing issue is observed.

image (7).png Screenshot 2025-01-01 174420.jpg
Devank_J by Associate II
  • 2328 Views
  • 3 replies
  • 0 kudos

Resolved! STM32C0116-DK: Problem with SPI + DMA at 24MBits/s

Hello!I am interfacing an ADS131M02 ADC to the STM32C0116-DK board using SPI for a project I am developing on live streamings. I am able to read SPI Data using the HAL polling functions (HAL_SPI_TransmitReceive), however that created unwanted delay b...

LabGluon_1-1767800596768.png LabGluon_2-1767800694645.png
LabGluon by Associate II
  • 630 Views
  • 5 replies
  • 4 kudos

Defective processors

Sequent Microsystems designs and sells Automation Systems using Raspberry Pi. All our products use STM processors. We use about 10,000 processors per year in different configurations. Generally we do not have any quality problems, but occasionally we...

mbeffa by Associate II
  • 1802 Views
  • 28 replies
  • 19 kudos

Resolved! Bit-banding Alternatives for Modern ARM Cores

Bit-banding Alternatives for Modern ARM Cores Background Information: The bit-banding feature available in ARM Cortex-M cores (ARMv7-M architecture including Cortex-M3 and Cortex-M4) provides hardware-level mapping of individual bits within a 1 MB me...

Komal_Y by Associate II
  • 1304 Views
  • 11 replies
  • 11 kudos

Resolved! Data transfer from SAI to DTCM using HPDMA not working

I am using a Nucleo-N657X0-Q board to prototype a data collection system that collects samples from an ADC connected to the SAI peripheral and places the results in RAM. If I use CPU AXI RAM0 as the destination this works correctly, but if I change t...

nige_w by Associate
  • 529 Views
  • 1 replies
  • 0 kudos

bootloader with 2 application

 I am working with an STM32F0 device and I want to implement a firmware update mechanism.My current plan is to split the internal flash into three regions:Bootloader: 0x08000000Application Slot 1 (App1): 0x08004000Application Slot 2 (App2): 0x0800800...

scotzap by Associate II
  • 737 Views
  • 5 replies
  • 3 kudos

STM32N6 power supply simplification

I am working on an STM32N6 hardware design, and have reviewed both development kit reference designs (MB1939/MB1940). Both designs use the same power supply scheme, when using internal SMPS it has 2x 3V3 regulators and 3x 1V8 regulators.I am interest...