STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI on STM32G071 not behaving as expected

Hi,i have  new design that i am migrating to the STM32G071 and having issues with the SPI1 port PB3,PB4,PB5. Changing CPOL and or CPHA during init code do not seem to have any impact, when powered down and restarted.I am seeing 9 clock pulses when se...

DS4_QuickPrint11.jpeg

Resolved! Power consumption of STM32H5 MCU for VIO Pins

Dear ST Team,I am using an STM32H5 series microcontroller in my design and I am trying to understand the overall power consumption contributed by different MCU interfaces.So far, I have identified the following:The typical maximum current on VDD, in ...

RajeshM by Associate II
  • 630 Views
  • 3 replies
  • 2 kudos

Resolved! STM32H753 FDCAN Bus Recovery

Good Morning,   I'm struggling with FDCAN Bus Recovery. The system we have to use consists of an STM32H753-based board and a 3rd party ECU, which is internally terminated via software. Our custom board is also terminated, resulting in the correct 60 ...

STM32H7R7 with APS6408 PSRAM

Hi there,I have been struggling with the PSRAM. I bought the STM32H7S78 board to pick up the know-how to understand how I should configure the PSRAM at XSPI1 via the EXT MEM manager at my own board. My clock speed is 200MHZ XSPI. PSRAM MPN: APS6408L-...

geriTricky_0-1767745738189.png

STM32H5 Flash layout obk and sytem

Is there a comprehensive single documentation source of the Flash layout for say, an STM32H563?The documentation I find is very opaque.  Questions I have at present (From a non secure perspective):1. Where is OBK located? (0x0BF0000 to 0x0BF9FFFF ???...

_EFrie by Senior
  • 688 Views
  • 2 replies
  • 0 kudos

firmware verification

Hello,I want to add a software update feature to my device, but I am unsure about the correct way to verify a newly installed firmware image. My goal is to make sure that the entire firmware has been written correctly and is not corrupted before the ...

scotzap by Associate II
  • 531 Views
  • 1 replies
  • 1 kudos