STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello World Error Program

I have a problem, where there's simply no error, but the output, is not showing on the screen. The system has detected the board, and all the correct steps are followed, even though, my hello world code is not been printed. I am using stm32cubeide ve...

Mohit79 by Associate
  • 444 Views
  • 3 replies
  • 1 kudos

Resolved! stm32 with 32 pins with FDCAN but without HSE?

HelloIm developing a CAN Bus node and with space constrains, so i ve looked in stm32 products and a qnf32 packages looked perfect for example stm32G0B1 has FDCAN. The problem...These QFN32 dont expose HSE pins. I just can use HSI with 16 MHz +- 1% wi...

ricardos by Associate II
  • 487 Views
  • 4 replies
  • 2 kudos

Using an STM32G484 OpAmp as a Shunt Sensor

 I'm developing a power bus manager where I monitor current and voltage drop across a shunt resistor. I chose the STM32G484 as the MCU because it has enough OpAmps and ADCs for my project.However, I have a question that might only be related to elect...

Resolved! STM32H56xx/STM32H57xx Stock and Lead Time

Hello,I would like to get information about the availability of the following devices:STM32H562IGK6 UFBGA 144 package (10 × 10 mm, 0.8 mm pitch)STM32H562IGT6Could you please clarify:Are these devices currently available in stock for production volume...

Resolved! Gravação mult

I would like to know how I can program 2 MCUs (stm32wb55cgu6) simultaneously.Currently, I am programming the FUS and BLE binaries (firmware developed by the company).We need to double production, but I can't program via DFU because an error always oc...

Resolved! Calibrating the STM32's real-time clock (RTC)

I have an STM32L011F4P6 with an RTC.  It is running at 3.3V and 16 MHz off the internal HSI RC clock.  The RTC is driven by a +/-20ppm 32.768 KHz crystal.  It is running at room temperature (23-25C).  After calibration, I am losing several seconds pe...

Resolved! STM32H723 SPI clock issue

In my project I've set the SPI clock to 125MHz; with a SPI prescaler value=4 all works good, when I set it to 2 the SPI stops working and ther is no clock signal.Any helps ? Thank youCarloV

carloV by Associate III
  • 897 Views
  • 11 replies
  • 2 kudos

Resolved! HAL_UART_Init() assert with LPUART at high baudrate

I call HAL_UART_Init() with LPUART1 at 20Mbaud but when I activate assertion it fail at IS_UART_BAUDRATE().The IS_UART_BAUDRATE() is not correct for LPUART that can have a baudrate up to 53.3 Mbaud.Also for UART, the comparaison in IS_UART_BAUDRATE()...

nicolas by Senior II
  • 498 Views
  • 4 replies
  • 1 kudos