2025-06-04 1:36 AM - last edited on 2025-06-04 2:45 AM by Andrew Neil
/*GLOBAL VARIABLE*/
#define ADC_CONVERTED_DATA_BUFFER_SIZE ((uint32_t) 100) /* Size of array aADCxConvertedData[] */
/* Variable containing ADC conversions data */
uint32_t aADCxConvertedData[ADC_CONVERTED_DATA_BUFFER_SIZE];
int isADCFinished = 0;
#define VDDA_APPLI (3300UL)
uint16_t uhADCxConvertedData_Voltage_mVolt = 0; /* Value of voltage calculated from ADC conversion data (unit: mV) */
/* Init variable out of expected ADC conversion data range */
#define VAR_CONVERTED_DATA_INIT_VALUE (__LL_ADC_DIGITAL_SCALE(ADC1, LL_ADC_RESOLUTION_14B) + 1)
/*************************************************************************************************/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the System Power */
SystemPower_Config();
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_GPDMA1_Init();
MX_ADC1_Init();
MX_ICACHE_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Initialize led */
BSP_LED_Init(LED_GREEN);
/* Initialize USER push-button, will be used to trigger an interrupt each time it's pressed.*/
BSP_PB_Init(BUTTON_USER, BUTTON_MODE_EXTI);
/* Initialize COM1 port (115200, 8 bits (7-bit data + 1 stop bit), no parity */
BspCOMInit.BaudRate = 115200;
BspCOMInit.WordLength = COM_WORDLENGTH_8B;
BspCOMInit.StopBits = COM_STOPBITS_1;
BspCOMInit.Parity = COM_PARITY_NONE;
BspCOMInit.HwFlowCtl = COM_HWCONTROL_NONE;
if (BSP_COM_Init(COM1, &BspCOMInit) != BSP_ERROR_NONE)
{
Error_Handler();
}
if (HAL_ADC_Start_DMA(&hadc1,
(uint32_t *)aADCxConvertedData,
(ADC_CONVERTED_DATA_BUFFER_SIZE)
) != HAL_OK)
{
Error_Handler();
}
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(isADCFinished == 1)
{
isADCFinished = 0;
uhADCxConvertedData_Voltage_mVolt = __LL_ADC_CALC_DATA_TO_VOLTAGE(ADC1, VDDA_APPLI, aADCxConvertedData[0], LL_ADC_RESOLUTION_14B);
if (HAL_ADC_Start_DMA(&hadc1,
(uint32_t *)aADCxConvertedData,
(ADC_CONVERTED_DATA_BUFFER_SIZE)
) != HAL_OK)
{
Error_Handler();
}
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef *hadc)
{
isADCFinished = 1;
}
static void MX_ADC1_Init(void)
{
/* USER CODE BEGIN ADC1_Init 0 */
/* USER CODE END ADC1_Init 0 */
ADC_ChannelConfTypeDef sConfig = {0};
/* USER CODE BEGIN ADC1_Init 1 */
/* USER CODE END ADC1_Init 1 */
/** Common config
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc1.Init.Resolution = ADC_RESOLUTION_14B;
hadc1.Init.GainCompensation = 0;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc1.Init.LowPowerAutoWait = DISABLE;
hadc1.Init.ContinuousConvMode = ENABLE;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.DMAContinuousRequests = ENABLE;
hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;
hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;
hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;
hadc1.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
Error_Handler();
}
/** Configure Regular Channel
*/
sConfig.Channel = ADC_CHANNEL_1;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_5CYCLE;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN ADC1_Init 2 */
/* USER CODE END ADC1_Init 2 */
}
/**
* @brief GPDMA1 Initialization Function
* @PAram None
* @retval None
*/
static void MX_GPDMA1_Init(void)
{
/* USER CODE BEGIN GPDMA1_Init 0 */
/* USER CODE END GPDMA1_Init 0 */
/* Peripheral clock enable */
__HAL_RCC_GPDMA1_CLK_ENABLE();
/* GPDMA1 interrupt Init */
HAL_NVIC_SetPriority(GPDMA1_Channel15_IRQn, 0, 0);
HAL_NVIC_EnableIRQ(GPDMA1_Channel15_IRQn);
/* USER CODE BEGIN GPDMA1_Init 1 */
/* USER CODE END GPDMA1_Init 1 */
/* USER CODE BEGIN GPDMA1_Init 2 */
/* USER CODE END GPDMA1_Init 2 */
}Edited to apply source code formatting - please see How to insert source code for future reference.
Solved! Go to Solution.
2025-06-04 5:28 AM
If resolution is 14 bits, the buffer data type should be uint16_t and the dma word size should be half-word.
2025-06-04 2:05 AM
This data not proper problem I've fixed. Now I've problem in reading 100 samples, I don't knwo why maximum 32 samples it's able to read
2025-06-04 5:28 AM
If resolution is 14 bits, the buffer data type should be uint16_t and the dma word size should be half-word.
2025-06-04 9:01 AM
@TDK Thanks for your reply I'm able to get it working