STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

"Optimized Resolution" options in CUBE ADC

I noticed some options in the CUBE IDE for my H745's ADCs labelled "ADC 12-bit optimized resolution" and likewise for 14 bits. I have searched the references and the internet and find no explanation of how "optimized resolution" differs from the regu...

VO by Associate III
  • 1816 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H7 USB VBUS sensing question

I am using the USB OTG FS on the STM32H7. My MCU is self powered, so I need to use VBUS sensing. Can a 3.3V signal be used for the VBUS sensing on PA9 or must it be 5V? Based on the linked forum, I believe 3.3V would work, but would like to confirm w...

Resolved! IWDG_STDBY ambiguity

Hi All,Please could somebody offer some words of wisdom to resolve the apparent ambiguity in the C0 datasheet, which on the one hand states that once IWDG is started it cannot be stopped, yet on the other hand offers a IWDG_STDBY bit in the OPTION re...

Resolved! stm32U585 + 2 x APS25608N OSPI - speed problems

Hai All!I use 2 pieces of APS25608N PSRAM on OSPI bus with memory mapped mode. The MCU run at 1.8V, 160MHz system clock. Previously, I used APS12808N at 80MHz and 3.3V VDD without any issues.Currently, the PSRAMs run at 50MHz, but need to speed up to...

ccuebler by Associate III
  • 820 Views
  • 5 replies
  • 2 kudos

STM32H750IBT6 Bootloader Problem

Hello everyone. I am trying to write a bootloader with STM32H750IBT6 and mt25ql512. I am trying to adapt the ExtMem_Boot example of STM32H750-DK to STM32H750IBT6 by modifying it, but I can't succeed. It doesn't make sense why STM32H750IBT6 does not w...

MKoca1_0-1729669938505.png
MKoca.1 by Senior
  • 3575 Views
  • 9 replies
  • 2 kudos

Supported PSRAM and Flash for the STM32N6xx

Hey guys, I'm looking for some suitable HexaSPI PSRAM and also the OctoSPI Flash for the STM32N645 board I am just building.. I cant find the parts used on the DK so do you have a list of supported memories? I need 256Mb PSRAM and will start with a 1...

RAdam.1 by Associate III
  • 826 Views
  • 5 replies
  • 4 kudos

Resolved! STM32G474RET6 VREF connection

Hello, I am planning to use the STM32G474RET6 and would like to confirm whether I can use the internal VREFBUF. This product's package is LQFP-64 and while reading the datasheet I noticed the note : ''The VREF+ pin is double-bonded with VDDA on some ...

Resolved! STM32H573 - missing BKPSRAM on memory map

Hello,The datasheet and reference manual are missing information about the 4 KB Backup SRAM in the memory map.Where can I find details about it?We need to use this memory in both Secure and Non-Secure projects.Thank you. 

RZub by Associate II
  • 291 Views
  • 3 replies
  • 1 kudos