STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Fixed point library

Posted on May 31, 2011 at 11:10Hi all, In my project, I am using a GPS to measure some distances, and some angles combined with a magnetometer. Therefore, I have to do a lot of floating point operations. It's dirty, it's slow, and it's taking a lot ...

Kuikui by Associate III
  • 3092 Views
  • 4 replies
  • 0 kudos

STM32F2XX Interrupts

Posted on May 30, 2011 at 20:36I have recently ported an application from the STM32F107 to the STM32F217 using the CrossWorks from Rowley tool chain.  My '107 project builds and runs correctly.  Amongst other things this project uses interrupts to m...

configuration register (stm32f107)

Posted on May 30, 2011 at 16:50hello, does anyone have already done this for GPIO? (port A, Port B, Port C, Port D and port E). a notepad will be enought. I'm programing on IAR embedded workbench (C laguage.) I need to transfert datas with USB and ...

STM32vl discovery as st-link

Posted on May 20, 2011 at 13:52Hello, I m trying to use the stm32vldiscovery board as a stand alone st-link programer, to program a stm32f207 microcontroller, through stm3220f board. As I plug the two board one to the other, before to start the debu...

weedoug18 by Associate II
  • 1665 Views
  • 3 replies
  • 0 kudos

VBAT Connection?

Posted on May 22, 2011 at 03:37Hi. The VL Manual (UM0919) says that by default solder bridge (SB1 VBAT) is factory set to be off. This should allow you to connect a battery to the board and run the real time clock when then board is powered off. The...

redgod9 by Associate
  • 3828 Views
  • 3 replies
  • 0 kudos

IAR + STLINK : Debugger error

Posted on May 19, 2011 at 10:44Hello, I am using stm32 discovery board + IAR 6.20 + STlink USB V2 When I want to download and debug the discovery application, I get the following errors: Thu May 19, 2011 10:36:43: Loaded macro file: C:\Program Files...

IAR says it programmed STM32VLDISCOVERY, but not really ??

Posted on May 19, 2011 at 05:04OK, with help from ST and IAR's technical support, I solved the build issues in IAR related to version conflicts between IAR6 and demo code/examples written for IAR5 (see previous post). Everything builds fine now.When...

davidm23 by Associate II
  • 1429 Views
  • 3 replies
  • 0 kudos