STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FFT problem

Posted on June 12, 2011 at 21:42I'm trying to calculate FFT of this signal (using Keil uVision and STM32F103VB:but the result looks like this:Here's the code://///////////////////////////////////////////////////////////////const int N=256;void fft()...

0690X00000602inQAA.gif 0690X00000602fQQAQ.jpg
deathclaw by Associate II
  • 1253 Views
  • 1 replies
  • 0 kudos

STM3210C_EVAL and LwIP implementation example (AN3102)

Posted on June 13, 2011 at 17:26Hi all. I tried to use the AN3102 example, which enable to implement the LwIP Ethernet stack on mu dedicated STM3210C_EVAL, composed of an STM32F107 µC. However, when I link it to the network or directly to my compu...

How to configure clock at 38 Khz with some other operation

Posted on June 11, 2011 at 00:22Hi All,      I want to configure the clock output at 32 Khz to 38 Khz in one of the pins and at the same time I want to send the data from USART. It is like two parallel operation; one pin is continuously generating t...

parag by Associate II
  • 1588 Views
  • 2 replies
  • 0 kudos

Write in Flash problem error

Posted on June 13, 2011 at 15:25  I'm trying to write a half word in the flash memory. Every time the system starts my code  write a half word in flash, but it works only the first time. In the others times the data is not store(PGERR error), and st...

reading Timer Status Reg kills timer?

Posted on June 09, 2011 at 22:22We are using the Atollic IDE.  After setting up TIM2,TIM3, or TIM4 to clock continuously.  We output the counter bits on PCx lines and monitor with a scope. We read the registers directly using: adr=0x40000???; data=*...

jlarsen by Associate
  • 981 Views
  • 2 replies
  • 0 kudos

How to configure clock at 38 Khz with some other operation

Posted on June 11, 2011 at 00:26Hi All,      I want to configure the clock output at 32 Khz to 38 Khz in one of the pins and at the same time I want to send the data from USART. It is like two parallel operation; one pin is continuously generating t...

parag by Associate II
  • 1120 Views
  • 1 replies
  • 0 kudos

GPIO AF mode

Posted on June 06, 2011 at 09:35Hi, Lets say i want to connect analog signal to ADC channel12 (which is default pin is PORTC-2). Should i configure GPIOC-2 mode as: GPIO_Mode_AIN or GPIO_Mode_AF_OD/PP? I suppose GPIO_Mode_AIN, so when do i use GPIO_...

ybitton by Associate II
  • 3608 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.