cancel
Showing results for 
Search instead for 
Did you mean: 

Overrun Error using USART1

Posted on May 16, 2011 at 15:09

Overrun Error using USART1

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Andrew Neil
Super User
Posted on May 17, 2011 at 14:35

    while( !(RCC_GetFlagStatus(RCC_FLAG_PLLRDY)== SET) );

 

Never have a busy-loop wait in an ISR!
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on May 17, 2011 at 14:35

[EDIT] : I found another problem not regarding the STM32. The post is to be closed Thanks all.

OK I will change this.

I forgot to say something, my USART is linked to the PC by a XBee module and it is also stood by as the STM32 is. I'm trying a solution which just comes to me. I'll shared it here if it works.

Posted on May 17, 2011 at 14:35

[EDIT] : I found another problem not regarding the STM32. The post is to be closed Thanks all.

 

OK I will change this.

 

 

I forgot to say something, my USART is linked to the PC by a XBee module and it is also stood by as the STM32 is. I'm trying a solution which just comes to me. I'll shared it here if it works.

Notwithstanding this apparent fix, you should always check for parity, framing, overrun, etc errors, and clear them by reading the data register. Even if you choose to ignore the error, it must be cleared before the USART will work properly again.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on May 17, 2011 at 14:35

Thanks for the advise.