Posted on May 17, 2011 at 13:23Last weeks i've got a few STM32F105 and F107 controllers. No bootloader ist working inside these devices (Rev. Z). No UART1, UART2 or USB-bootloader port is working. I've tried with different crystals, 8MHz, 25MHz. No ...
Posted on May 17, 2011 at 13:21Hello, it is the same problem here. I also have got samples from ST, STM32F105RC (64 pins), STM32F107VB (100 pins, rev.Z). No Bootloader-Port is working correct: USART1 doesn't work cause of conflict with OTG-pins. No ...
Posted on May 17, 2011 at 13:15Hello, a new STM32-programmer tool for the STM32 integrated bootloader is online. You can use this software with a standard USB to serial interface but it works more perfect with a special hardware which controls the R...