STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM322xg Eval board SDIO Problems

Posted on October 05, 2011 at 19:18Hello all, I have search through the forums and google for the exact problem I am having to no avail. The issue I am having is regarding finding the filesystem on the SD card, in particular the check_fs function in...

stbbrad3 by Associate II
  • 5225 Views
  • 16 replies
  • 0 kudos

Keil MDK-ARM V4.14.4.0 return error 65: access violation

Posted on January 28, 2011 at 10:39 Hello, I try to debug and simulate the discover project on MDK-ARM evaluation IDE. I have no hardware. So i just want to test debug and simulation. Here below the error message after build and start ...

RomainR. by ST Employee
  • 8975 Views
  • 15 replies
  • 0 kudos

ST-One: STM32F4xx ADC Channels

Posted on October 18, 2011 at 03:34The data sheet for the STM32F4 series states that 24 external ADC input channels are available, but I can find only 23 in the pin assignments. ADC3_IN8 appears to be missing. The F4 reference manual (RM0090) descri...

Retarget scanf stm32 atollic

Posted on October 17, 2011 at 18:59Hi guys,I am trying to retarget scanf for USART1 of STM32 using Atollic. I think the utilized toolchain makes use of _read_r for the scanf (please verify if possible). So I need a new definition of _read_r. Any ide...

Cygwin gcc tool-chain for bare metal STM32?

Posted on October 17, 2011 at 17:06Hi all, I noticed that arm-elf-gcc, arm-elf-binutils and arm-elf-newlib are included as pre-built packages with Cygwinports. ftp://sourceware.org/pub/cygwinports/portslist.txt Can this tool-chain be used for STM32...

FreeRTOS MPU on stm32

Posted on October 07, 2011 at 10:52Hi, I am desperately trying to get the FreeRTOS MPU port running on my STM3210e-Eval Board. (Yes I am sure that my MCU has the MPU ;) ). I cannot find a working linkerscript for the GCC Toolchain. Has anyone ever...

tor by Associate
  • 1359 Views
  • 2 replies
  • 0 kudos

TotalFifoSize in STM32f107

Posted on October 17, 2011 at 17:52I have been looking at the USB OTG Libraries for the 105/7 and I've come across the variable  TotalFifoSize.  It's set to 320, when using the Full speed core.I was wondering if anyone knew if this was because of a ...

Wii Motion Plus (Cant connect)

Posted on October 17, 2011 at 00:14The original post was too long to process during our migration. Please click on the attachment to read the original post.

VCP Demo

Posted on May 05, 2011 at 11:13VCP Demo

greg_t by Associate II
  • 2295 Views
  • 5 replies
  • 0 kudos

I2C rev. 03 19 june 2007

Posted on September 30, 2011 at 20:39Hi all,does anyone know if STM32 family I2C master supports 24-bit device ID reading from an I2C slave? I have a slave compliant to I2C rev 03 standard and I need to read it's device ID. Please help, have you any...

brazov22 by Associate II
  • 2205 Views
  • 5 replies
  • 0 kudos