Posted on May 17, 2011 at 13:27thanks for your answer.I have read the page,It seems that Cycle counter statistics is not supported by all debug tools at present.It is avaliable only in simulator mode. though it is really important in arith developme...
Posted on May 17, 2011 at 13:27hello, I need to use profiling tool to improve arith performance,and I get the infomation that J-LINK can support profiling tool in hardware simulation. However,when push the start button of profiling tool window,only...
Posted on May 17, 2011 at 13:21STone-32, thanks for your advices, I have checked the external circuit and found the problem actually come from the circuit.
Posted on May 17, 2011 at 13:21hello, I meet this problem when using gpio pin PA11 and PA12, this two pins are shared as USART1's CTS and RTS.when sending data on USART1,pulses could be detected on this two pins.However, I didn't enable CTS and RTS....