STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Yagarto vs Raisonance

Posted on December 16, 2011 at 06:51I'm using a makefile to build my application - I'm not a huge fan of IDE's.By setting my PATH environment variable (in Win32 system) to the Raisonance toolchain everything builds fine and runs fine on my STM32F2.B...

carl2399 by Associate III
  • 5005 Views
  • 11 replies
  • 0 kudos

What is the SPI1 address for the DMA controller?

Posted on December 17, 2011 at 04:36I am attempting to transmit SPI1 data using DMA2. What is the SPI1 PeripheralBaseAddr to be used in the following statement? DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)SPI1_DR_ADDRESS;

CC Timer Interrupt (STM32F102RBT6)

Posted on December 16, 2011 at 19:19Using a general purpose timer (TIM3), with a constant frequency I would like to be able to occasionally generate an interrupt on CC3 using a variable count for CCR3.  I do not want to generate a PWM signal or chan...

jmorton by Associate II
  • 1993 Views
  • 2 replies
  • 0 kudos

STM32w108 delay function with Ember stack

Posted on December 16, 2011 at 15:09hi, i have a problem with delay time function of the STM32W108 and EmberZnet stack. so I want a delay time of more than 10 seconds. I used the HAL library and especially the function: halCommonDelayMilliseconds();...

w23 by Associate II
  • 1944 Views
  • 5 replies
  • 0 kudos

Servo control using STM32VLDiscovery

Posted on October 13, 2011 at 14:18Hi all,I want to run a servo using the STM32 Discovery, if you have a suggestion program torun the servo?or you have a simple code to run the servo on the STM32 DiscoveryThank youRegards,Endy

How are Interrupt Handlers placed in the vector table?

Posted on December 15, 2011 at 01:40I am testing interrupts in general, TIM3_IRQHandler( ) specifically. I am trying to create a new handler for TIM2. I see in the TIM_TimeBase example where this is defined. How and where does the address of the IRQ...

STM32F1/F4 incompatible I/O

Posted on December 08, 2011 at 19:34From their respective RMs: STM32F1... 0x4002 2000 - 0x4002 23FF Flash memory interface STM32F4... 0x4002 2000 - 0x4002 23FF GPIOI Thus a project predicated on STM32x compatibility must have at least different I/O ...

picguy2 by Associate II
  • 1606 Views
  • 4 replies
  • 0 kudos

SD Card on STM32VL-Discovery

Posted on December 13, 2011 at 09:14Hi Has anyone got an SD Card or MMC talking to the Discovery board yet? I can't find much information on the forum. Can anyone, point me in the right direction?Thanks in advanceAmir #sd-card #mmc #stm32-discove...

apatel by Associate II
  • 1813 Views
  • 3 replies
  • 0 kudos