STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About st peripherial library

Posted on December 18, 2011 at 20:24Hello, Im trying to use st standart peripherial libraries. In my project im adding stm32f10x.h file ,and also i uncommented #include ''stm32f10x_rcc.h'' line. There is a question at this point. When i activate #i...

DMA transfer from ADC to array in memory

Posted on December 13, 2011 at 15:35Hello there, I'd like to set up an ADC and DMA so that converted data is directly written into an array in memory. I modified the ADC3_DMA example but it doesn't work correctly. I replaced ''ADC3ConvertedValue'' ...

raffael by Associate II
  • 2343 Views
  • 2 replies
  • 0 kudos

USB Tx problem after wakeup

Posted on December 15, 2011 at 20:30Hello, I'm trying to put USB communication in suspend mode, but when I force wake up, just can read data from PC, but nothing is sent. The interrupt for correct Tx transmition isn't fired. The end point is well co...

ADC resolution for stm32f205

Posted on December 19, 2011 at 10:40Hi, ADC resolution is working for ''ADC_Resolution_6b'' and ''ADC_Resolution_12b'' but not working for ''ADC_Resolution_8b'' and ''ADC_Resolution_10b'' resolutions, they're same with 12-bit resolution. Does anyone...

acihana by Associate II
  • 1611 Views
  • 3 replies
  • 0 kudos

quadrature encoder

Posted on December 18, 2011 at 01:56Hi, I am trying to get the quadrature encoder working.  I found and copied code from these forums for setting it up with a different micro controller but the one on the STM32F4 does not support RCC_APB2Periph_GPIO...

stm32l beginner questions

Posted on December 16, 2011 at 16:33Hello,I've recently bought a stm32l-discovery board and I want to start developing for the onboad processor. I  have some previous experience with 8bit atmel microcontrollers but not with (32bit) ARM processors.I ...

luc2 by Associate
  • 799 Views
  • 2 replies
  • 0 kudos

LSI as RTC clock

Posted on December 15, 2011 at 11:24Hi , Is it possible to run RTC with 40khz LSI when power is off and CPU works on battery only? #rtc #lsi

STM32F105 USB Speed, Fifo size

Posted on December 14, 2011 at 20:52Dear all, I've not found a related topic. Right now I've checked with the demo of mass storage device the possible maximum transfer speed. And it looks like ~500kByte/s, for writing to the device. The define at us...

elgerta by Associate II
  • 1559 Views
  • 2 replies
  • 0 kudos