cancel
Showing results for 
Search instead for 
Did you mean: 

H-Bridge circuit for Advanced Timer using a DC brush motor

jveith
Associate II
Posted on June 08, 2011 at 16:23

anybody knows a application note for a circuit with 4 N-channel mosfets or 2 P/N channel pairs. My DC brush motor is about 24V 6 Amp and I prefere to use the complementary outputs for Timer 1 / Timer 8 with programmable deadtime instead of integrated H-Bridge

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0