STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to compute filter coefficients?

Posted on December 20, 2011 at 14:26Hi every stm32 fan, In my application I am sampling my input signal at 8KHz and now I need to filter out my samples in order to remove high components. Is there a software tool which computes the coefficients of a...

STM32F4-Discovery Base Board with BB3U

Posted on December 22, 2011 at 23:09I have built a baseboard for the STM32F4 Discovery module.  It has two RS232 ports and two 50-pin headers allow easier connection to the other pins. I have some photos on my blog:http://kornakprotoblog.blogspot.co...

kornak by Associate II
  • 671 Views
  • 0 replies
  • 0 kudos

5V in 3.3V logic level when powering F205 through USB OTG HS

Posted on December 21, 2011 at 18:54Hi We have an odd problem. We have a custom F205RBT6 based board. It can be powered through separate 5V pins or USB. The 5V goes to a 800mA linear regulator which then provides 3.3V to the F205. We have an extra l...

tuomas by Associate II
  • 1689 Views
  • 4 replies
  • 0 kudos

UART2 RX TX initialization

Posted on December 18, 2011 at 16:29UART2 RX TX initialization-how to use?Hello, I have problem with initialization UART2 in my project(STM8S105). Below you can see part of my code, what am i doing wrong? I'm trying to send sign to LCD display. [cod...

pietruha8 by Associate II
  • 2843 Views
  • 6 replies
  • 0 kudos

The output signals at the maximum frequency.

Posted on December 21, 2011 at 12:45How can I synchronize the timer output with a maximum frequency PLL, ie 168 MHz.  In my example I set the timer to slow generate an interrupt, which run fast timer for generating a single pulse duration of 6 ns, b...

scolonel by Associate
  • 1758 Views
  • 3 replies
  • 0 kudos

STM32F4 RTX & FPU

Posted on December 21, 2011 at 15:59I had a few general questions regarding the RTX RTOS on an STM32F4.  What are the limitations with regard to the FPU while using RTX?  Is it possible to switch tasks while in the middle of a floating point operati...

STM32-VLDiscovery UART between Eval & PC Problem

Posted on December 19, 2011 at 17:20 Hi I trying to access UART connection between eval board and pc. I am using uart 1 on PA9 and PA To change the signals i am using a MAX From the eval board to the pc the signals are correct, but b...

bandido1 by Associate II
  • 1259 Views
  • 2 replies
  • 0 kudos

Compiling the Demo Software

Posted on November 01, 2011 at 15:00I have been trying to compile the Demo for the STM32F4 Discovery board and I have been getting errors for Missing header files. Does anyone know where I can get the following header files? armcm4.h arm_math.h Than...

mnmis by Associate II
  • 2289 Views
  • 5 replies
  • 0 kudos